TOUCH Screen coordinate Jitter .CRAZY!!!!!

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

TOUCH Screen coordinate Jitter .CRAZY!!!!!

ソリューションへジャンプ
3,194件の閲覧回数
peigao
Contributor I

we used the i.MX536&DA9053 design a hand-in meter.it has an 5.6" LCD SCREEN combine with a touch screen .we use the DA9053 touch screen interface.

in the HIM. a visual keyboard exist. but when we use finger touch the visual keyboard frame.it keep jitter and never-ending. in the SCH ,the touch screen path is very short.we use 4-cap on the X+,X-,Y+,Y- to filtering the jitter. but has no effect.evreyone,have u used have this problem?

ラベル(3)
0 件の賞賛
返信
1 解決策
2,078件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

1. please add the tslib package in the Package List in LTIB Configuration.

2. please try to delete the pointercal file and do the calibration again.

Before run the ts_calibrate, please try to "export" the followings:

  export TSLIB_ROOT=/usr

  export TSLIB_TSDEVICE=/dev/input/event2     (please change it if your touchscreen device node is different)

  export TSLIB_CALIBFILE=/etc/pointercal

  export TSLIB_CONFFILE=$TSLIB_ROOT/etc/ts.conf

  export TSLIB_PLUGINDIR=$TSLIB_ROOT/lib/ts

  export TSLIB_CONSOLEDEVICE=none

  export TSLIB_FBDEVICE=/dev/fb0

  The existing /etc/ts.conf should look like this.

  module_raw input

  module pthres pmin=1

  module variance delta=30

  module dejitter delta=100

  module linear

3. If the GUI is Ubuntu, please read the i.MX5x_EVK_Ubuntu_9.10_StartupGuide.pdf or i.MX5x_EVK_Ubuntu_10.04_StartupGuide.pdf

4. you can try to use the evtest to check the touchscreen input.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,079件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

1. please add the tslib package in the Package List in LTIB Configuration.

2. please try to delete the pointercal file and do the calibration again.

Before run the ts_calibrate, please try to "export" the followings:

  export TSLIB_ROOT=/usr

  export TSLIB_TSDEVICE=/dev/input/event2     (please change it if your touchscreen device node is different)

  export TSLIB_CALIBFILE=/etc/pointercal

  export TSLIB_CONFFILE=$TSLIB_ROOT/etc/ts.conf

  export TSLIB_PLUGINDIR=$TSLIB_ROOT/lib/ts

  export TSLIB_CONSOLEDEVICE=none

  export TSLIB_FBDEVICE=/dev/fb0

  The existing /etc/ts.conf should look like this.

  module_raw input

  module pthres pmin=1

  module variance delta=30

  module dejitter delta=100

  module linear

3. If the GUI is Ubuntu, please read the i.MX5x_EVK_Ubuntu_9.10_StartupGuide.pdf or i.MX5x_EVK_Ubuntu_10.04_StartupGuide.pdf

4. you can try to use the evtest to check the touchscreen input.

0 件の賞賛
返信