TLV320AIC3104-Q1: Need Help to solve Error:error at snd_soc_component_update_bits and error at soc_c

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TLV320AIC3104-Q1: Need Help to solve Error:error at snd_soc_component_update_bits and error at soc_c

3,282 Views
divyeshmarne0
Contributor III

Hi Team,

CODEC: TLV320AIC3104 External Codec.

CHANGES:

+ sound-tlv320aic3x {
+ compatible = "simple-audio-card";
+ simple-audio-card,name = "tlv320aic3x-Codec";
+ simple-audio-card,format = "i2s";
+ simple-audio-card,frame-master = <&cpudai1>;
+ simple-audio-card,bitclock-master = <&cpudai1>;
+
+ simple-audio-card,widgets =
+ "Line", "Line Out",
+ "Line", "Line In",
+ "Headphone", "Headphone Jack",
+ "Speaker", "speaker";
+ simple-audio-card,routing =
+ "Line Out", "HPLCOM",
+ "Line Out", "HPRCOM",
+ "LINE1L", "Line In",
+ "LINE1R", "Line In",
+ "Headphone Jack", "HPLOUT",
+ "Headphone Jack", "HPROUT",
+ "speaker", "LLOUT",
+ "speaker", "RLOUT";
+
+ cpudai1: simple-audio-card,cpu {
+ sound-dai = <&sai1>;
+ dai-tdm-slot-num = <2>;
+ dai-tdm-slot-width = <32>;
+ };
+
+ simple-audio-card,codec {
+ sound-dai = <&tlv320aic3x>;
+ clocks = <&clk IMX8MM_CLK_SAI1_ROOT>;
+ };
+ };

BUS-I2C3

+ tlv320aic3x: codec@18 {
+ compatible = "ti,tlv320aic3104";
+ reg = <0x18>;
+ #sound-dai-cells = <0>;
+ reset-gpios = <&gpio4 28 GPIO_ACTIVE_LOW>;
+ DRVDD-supply = <&reg_3p3v>;
+ AVDD-supply = <&reg_3p3v>;
+ IOVDD-supply = <&reg_3p3v>;
+ DVDD-supply = <&reg_1p8v>;
+ };

Need your help to solve following errors

E tlv320aic3x-codec 2-0018: Unable to sync registers 0x3-0x3. -6
E tlv320aic3x-codec 2-0018: ASoC: error at soc_component_write_no_lock on tlv320aic3x-codec.2-0018: -6
E tlv320aic3x-codec 2-0018: ASoC: error at soc_component_write_no_lock on tlv320aic3x-codec.2-0018: -6
E tlv320aic3x-codec 2-0018: Unable to sync registers 0x3-0x3. -6
E tlv320aic3x-codec 2-0018: ASoC: error at soc_component_write_no_lock on tlv320aic3x-codec.2-0018: -6
E tlv320aic3x-codec 2-0018: ASoC: error at soc_component_write_no_lock on tlv320aic3x-codec.2-0018: -6

Latest LOGS:

[ 75.803029] i2c i2c-2: Divyesh <i2c_imx_xfer_common>
[ 75.808085] i2c i2c-2: Divyesh <i2c_imx_start>
[ 75.812859] i2c i2c-2: Divyesh <i2c_imx_xfer_common> transfer message: 0
[ 75.819683] i2c i2c-2: Divyesh <i2c_imx_write> write slave address: addr=0x30
[ 75.826995] i2c i2c-2: Divyesh <i2c_imx_trx_complete> TRX complete
[ 75.833236] i2c i2c-2: Divyesh <i2c_imx_acked> No ACK
[ 75.838413] i2c i2c-2: Divyesh <i2c_imx_xfer_common> exit with: error: -6
[ 75.845333] tlv320aic3x-codec 2-0018: ASoC: error at snd_soc_component_update_bits on tlv320aic3x-codec.2-0018: -6
[ 75.855766] i2c i2c-2: Divyesh <i2c_imx_xfer_common>
[ 75.860781] i2c i2c-2: Divyesh <i2c_imx_start>
[ 75.865489] i2c i2c-2: Divyesh <i2c_imx_xfer_common> transfer message: 0
[ 75.872335] i2c i2c-2: Divyesh <i2c_imx_write> write slave address: addr=0x30
[ 75.879741] i2c i2c-2: Divyesh <i2c_imx_trx_complete> TRX complete
[ 75.885980] i2c i2c-2: Divyesh <i2c_imx_acked> No ACK
[ 75.891086] i2c i2c-2: Divyesh <i2c_imx_xfer_common> exit with: error: -6
[ 75.897933] tlv320aic3x-codec 2-0018: ASoC: error at snd_soc_component_update_bits on tlv320aic3x-codec.2-0018: -6

Please check Image and Boot logs:

TAG to search in txt file: divyeh ,tlv320aic.

I think master IMX8MMEVK is not able to communicate with slave address 00011000 (0x18).

Question is: If we are using TLV320AIC3104EVM Board only then what are the changes needed.

Currently We are giving MCLK,BCLK,WCLK,DIN,DOUT,SCL,SDL and 5V to TLV320AIC3104EVM board. In order to set slave address 0x18 ,do we need to make any configurations?

Could you please explain what other changes need to be done.

NOTE: TRIED WITH 1B slave address.

0 Kudos
Reply
3 Replies

3,261 Views
igorpadykov
NXP Employee
NXP Employee

Hi Divyesh

 

>I think master IMX8MMEVK is not able to communicate with slave address 00011000 (0x18).

>Question is: If we are using TLV320AIC3104EVM Board only then what are the changes needed.

 

one can look at sect.4.2 Interface Selection TLV320AIC3104EVM User Guide

TLV320AIC3104EVM-PDK User's Guide

 

Best regards
igor

0 Kudos
Reply

3,250 Views
divyeshmarne0
Contributor III

Hi, 

Section 4.2 has GUI related changes. 

We are not using any software for testing. 

We have direct connection to imx8mm evk board. 

Note: Not using USB MODEMV board for aic3104evm. 

0 Kudos
Reply

3,242 Views
igorpadykov
NXP Employee
NXP Employee

may be suggested to apply to tech support vendor of that board:

https://ticsc.service-now.com/csm?_ticdt=MTYzOTI5ODk3M3wwMTc4YTY5OTVmZGMwMDMzM2IwYzlkMzAzYzljMDAwNGQ...

 

Best regards
igor

 

 

 

0 Kudos
Reply