Hi Alejandro,
Thank you for your response.
I also have Ubuntu running in a virtual machine an I can successfully
connect to the tftp server running on this machine, but when I try to
connect to the tftpd32 process running on my XP laptop it doesn't
connect - can't see any logging messages. Thus it is connecting with
Ubuntu, I am happy with that for the moment, but I have to start the
virtual machine each time for this process.
Tftpd32 offers a tftp client itself on a different tab. If I use this
client to connect and download from the tftpd32 server it connects and
loads, so I think this server should be running and working - but it
doesn't connect from SABRE board.
Maybe there's a firewall blocking from external device - I don't know at
the moment.
I can live with the Ubuntu solution, but if someone knows how to solve
the tftpd32 issue, I would like to know.
I am using the SABRE 4core board, but haven't tested with other clients,
only from u-boot.
Kind regards
Juergen