TFT3P5581-T MIPI display help

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

TFT3P5581-T MIPI display help

2,255件の閲覧回数
ferfersan6
Contributor I

 

Hello.

I just acquired the MIPI display that I mention in the subject. Is there any information about setting it up? I am really new to displays and if somebody suggests me "getting started" information I would be very pleased. I have been researching the whole internet but did not found nothing really interesting.

I am working on a i.MX7ULP-EVK so it has a MIPI-DSI connector which matches perfectly with the display. 

I have read about the device-tree and the MIPI driver on the Linux Reference Manual but I do not know how to take that information and make changes on my board. 

Thanks in advance.

タグ(3)
0 件の賞賛
返信
3 返答(返信)

2,243件の閲覧回数
igorpadykov
NXP Employee
NXP Employee
0 件の賞賛
返信

2,229件の閲覧回数
ferfersan6
Contributor I

 

Thank you for your response.

The image already had the .dts you mentioned. Is there any example program to use the display? I would like to take it as reference for the future.

 

Regards.

0 件の賞賛
返信

2,223件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

>Is there any example program to use the display?

 

examples are linux fbdev display framework,

please look at sect.6.4.2 MIPI DSI Interface i.MX Linux Reference Manual​

simple unit test

https://source.codeaurora.org/external/imx/imx-test/tree/test/mxc_fb_test/doc/FSL-UT-FB-003.txt?h=im...

 

Best regards
igor

0 件の賞賛
返信