I plan to use the i.MX 8m processor for the video controller. I will use OLED panel as display. So I have to solve the image-sticking problem, is there any way like the program or API that NXP provides to solve image-sticking?
Image Sticking is a phenomenon in which certain pixels are burn-in due to the functional nature of self-luminous OLEDs. For example, if a fixed image, such as the logo of a broadcasting company, is continuously displayed for a very long time, the logo image will remain physically blurred in that part.
pls tell me what your test steps, then I can reproduce this issue on my board, your information is too limitied , pls give me more detailed information you could, what bsp version and how to reproduce this on nxp imx board
what image-sticking do you mean? could you give me more detailed use case?
Image Sticking is a phenomenon in which certain pixels are burn-in due to the functional nature of self-luminous OLEDs. For example, if a fixed image, such as the logo of a broadcasting company, is continuously displayed for a very long time, the logo image will remain physically blurred in that part.