System hang when using devmem2 to read GPMI registers

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

System hang when using devmem2 to read GPMI registers

3,836 Views
abutter
Contributor I

When running devmem2 0x01806000 w to check GPMI registers, the system seemed hang, there is no response when I input something on serial console.

I tried other register, devmem2 works and I could read 0x01806000 in u-boot using md command:

root@imx6ul-var-dart:~# devmem2 0x020c4068 w
/dev/mem opened.
Memory mapped at address 0x76f5e000.
Read at address  0x020C4068 (0x76f5e068): 0xC0C00F0F
root@imx6ul-var-dart:~# devmem2 0x01806000 w
/dev/mem opened.

I suspect if the clock for GPMI is disabled, but before reading the GPMI register, I run nandtest command, no crash or hang was seen.

Any suggestion is appreciated.

Thanks.

Labels (2)
0 Kudos
Reply
2 Replies

3,609 Views
igorpadykov
NXP Employee
NXP Employee

Hi abutter

one can look at similar problem on below link, check register with memtool

Unable to access I.MX6ULL memory map registers using devmem2 - fsl-yocto-L4.9.11_1.0.0.tar 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

3,608 Views
abutter
Contributor I

memtool also cause hang. I would try on other board to check if it is caused by the NAND and its driver.

I also thought it would be because of disabled clocked, I would try to the registers later.

0 Kudos
Reply