System Controller Firmware API Reference Guide i.MX8

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

System Controller Firmware API Reference Guide i.MX8

6,387 Views
ajmalali
Contributor III

Hi

Where can i get the "System Controller Firmware API Reference Guide i.MX8 QXP/DX". Can someone point me to the link?

Regards,

Ajmal

Tags (3)
0 Kudos
Reply
2 Replies

5,160 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ajmal

please look at SCFW porting kit

Alpha / Beta BSPs for Microprocessors|NXP 

pastedImage_2.jpg

other documentation for prerelease products is available from nxp local marketing office.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

3,939 Views
dry
Senior Contributor I

Its year 2022, and reading UG for the chip still referrers to that guide with no link.

Where do I find this guide, which hopefully helps me to set MUX for GPIO's, into direct control for output ..?

 

Tags (1)
0 Kudos
Reply