Synthesis of one IPU .

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Synthesis of one IPU .

862件の閲覧回数
takashitakahash
Contributor III

Hi community.

How many  synthesis  of one IPU  can be out put  number of frame plane and the upper limit pixsel size and frame rate FPS(Frame par second)?

One of IPU in a Plane capable of synthesizing the number, size, and frame rate

Use the divide within the maximum output of the DP 240Mp/s?

Use the 4 Plane for all 30 fps @ 1920 x 1080.

It would require approximately  more than 400Mp/s over, but one IPU has 240Mp/s.

Is it cannot be synthesized?

In this case how many synthesize screen plane?

ラベル(2)
0 件の賞賛
返信
1 返信

819件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Takashi

you are right, for 4 planes output rate will be less, for capabilities one can look at

presentation below p.58

A Deep Dive into Image Processing for i.MX 6 Series Applications Processors

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信