Synthesis of one IPU .

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Synthesis of one IPU .

922 Views
takashitakahash
Contributor III

Hi community.

How many  synthesis  of one IPU  can be out put  number of frame plane and the upper limit pixsel size and frame rate FPS(Frame par second)?

One of IPU in a Plane capable of synthesizing the number, size, and frame rate

Use the divide within the maximum output of the DP 240Mp/s?

Use the 4 Plane for all 30 fps @ 1920 x 1080.

It would require approximately  more than 400Mp/s over, but one IPU has 240Mp/s.

Is it cannot be synthesized?

In this case how many synthesize screen plane?

Labels (2)
0 Kudos
Reply
1 Reply

879 Views
igorpadykov
NXP Employee
NXP Employee

Hi Takashi

you are right, for 4 planes output rate will be less, for capabilities one can look at

presentation below p.58

A Deep Dive into Image Processing for i.MX 6 Series Applications Processors

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply