Synchronous Burst Mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Synchronous Burst Mode

1,957件の閲覧回数
dasnavissabiya
Contributor I

Hello,

I am access FPGA connected over EIM interface in iMX6 Sabre-SDB.

The EIM registers are configured as follows:

EIM_CSnGCR1 : 1191503f

EIM_CSnGCR2 : 1002

EIM_CSnRCR1 : 7101111

EIM_CSnRCR2 : 1c

EIM_CSnWCR1 : 6209249

EIM_CSnWCR2 : 0

When i tried to long read (using readl), burst read is not happening. Instead sequential reads are happening. In short, the address gets incremented and sequential 16-bit read occurs.

I observed this behavior using logic analyzer.

Please let me know, if the configuration above is correct(for synchronous burst read in multiplexed mode) ?

What else am i missing?

Is there any sample code for synchronous burst read?

Thank you in advance.

Regards,

Dasnavis Sabiya

ラベル(3)
1 返信

1,525件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Dasnavis

EIM does not produce burst from multiple single reads, master

should produce burst (for example from arm using ldm/stm instructions or

sdma transfer). Conditions for burst termination are given in

sect.22.5.3 Burst Mode (Synchronous) Memory Operation

i.MX6DQ Reference Manual (rev.2  7/2014)

http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf

As example one can look at attached i.MX53 tests, seems settings

can be reused for i.MX6.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信