Switching Exception Level EL3 to EL1 in IMX8M

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Switching Exception Level EL3 to EL1 in IMX8M

2,583 Views
Hariharan1
Contributor III

in Arm Cortex A53. I was competed Enabled Quad core, now I want to trigger interrupt. The interrupt present in exception level 1 (EL1). There is an issue while I am switching EL3 to EL1. When I jump to el1 entry symbol it is going to hanging in synchronous exception handler(cxsynx). Where I did mistake in this scenario.kindly let me know

0 Kudos
Reply
2 Replies

2,549 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

EL1 is the level that priveldged parts of the OS kernels use, so for example, Linux Kernel code will run with EL1 priveledges

AArch64 has a dedicated register (CurrentEL) that we can read to figure out our the current EL. CurrentEL is a system register and we should use a special instruction mrs to read such system registers, so the code starts like this:

mrs x0, CurrentEL

This instruction will read the content of the CurrentEL to a general purpose register x0. The register CurrentEL is a 64-bit one, but most of the bits are hardwired to be 0 and only bits 2 and 3 contain the actual EL value

So now we need to test if the value we read from CurrentEL is:

  • equal to 8 - nothing for us to do, we are already at EL2
  • smaller than 8 - to late for us to do anything, we are in EL1 or EL0
  • higher than 8 - we are in EL3 and have to jump to EL2.

NOTE: remember that the EL value is stored in bits 2 and 3, that’s why we compare to 8 and not to 2 (8 is just 2 shifted by 2 bits).

Putting everything together we get the following:

    mrs x0, CurrentEL
    cmp x0, #0b1000  // remember the EL value is stored in bits 2 and 3
    beq in_el2
    blo in_el1

in_el3:
    // Put code switching from EL3 to EL2 here

in_el2:
    // This code will run at EL2

in_el1:
    // We are in EL0 or EL1, so we probably should report an error here

 

Regards

0 Kudos
Reply

2,537 Views
Hariharan1
Contributor III

mov x3, #(SCR_EL3_RW | \
SCR_EL3_SMD | \
SCR_EL3_NS) // Set NS bit, to access Non-secure registers
msr SCR_EL3, x3
mov x0, #(HCR_EL2_RW)
msr hcr_El2, x0
// Initialize the SCTLR_EL1 register before entering EL1.
MSR SCTLR_EL1, XZR

mov x0, #15
msr ICC_SRE_EL2, x0
isb
msr ICC_SRE_EL1, x0 // Non-secure copy of ICC_SRE_EL1

//
// Get the current state and exception level
mrs x0, CurrentEL
and x1, x0, #0xC
lsr x1, x1, #2



// Set the target PC_EL1 to the exception handler address
adr x3, el1_entry_aarch64
msr elr_el3, x3

mrs x1, SPSR_EL3
msr daifset, #0xF

mrs x2, SPSR_EL3
mov x2, #0x3C5
msr SPSR_EL3, x2

//Enabling IRQ by clearing bit
mrs x0, daif
bic x0, x0, #(1 << 7)
msr daif, x0

//Disabling IRQ by masking bit
mrs x0, daif
orr x0, x0, #(1 << 7)
msr daif, x0

// Switch to EL1
eret

el1_entry_aarch64:
ldr x0, =__stack
Mov sp, x0
bl main

This is my code. I was checked currentel register, it contain exception level 3(EL3). Once jump into el1entry function after that CPU gets hanging. Not even check esr_el1 register. Can you check it, what I need to change in this code?

0 Kudos
Reply