Suspend-to-RAM debugging

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Suspend-to-RAM debugging

2,547 Views
harald_krapfenb
Contributor III

Hello,

I have a custom i.MX53 board where suspend-to-RAM is not working properly, i.e. the board won't wake up; and I believe it crashes even before going to suspend anyway.

Linux Standby mode works and the board wakes up again.

I use 2.6.35, from 11.05 ER Freescale BSP.

Stepping through the assembly code before the WFI instruction is executed within DS-5, I found that the problem is in cpu_do_suspend_workaround(), file arch/arm/mach-mx5/suspend.S.


More detail, the mx53_force_ddr_selfrefresh section goes wrong when the FDVFS bit in M4IF_CR0 register is set.

mx53_force_ddr_selfrefresh:
    PM_SET_ADDR_REG MX53_M4IF_CR0_FDVFS_ADDR, r4
    ldr r5, [r4]
    orr r5, r5 , #0x800
    str r5, [r4]

The processor locks up so I need to power-cycle it; and the debugger disconnects. I believe, sending low-power request to the fast channel of the EXTMC should not influence the JTAG clocks/connection. Who knows better?

Is there an idea by anyone what could go wrong? The manual's information about the FDVFS bit is rather sparse; I don't know what the M4IF does in background before it should acknowledge the low power state.

Thanks!

0 Kudos
Reply
3 Replies

2,285 Views
VincentChen
Contributor I

Sorry, I don't know the function of cpu_do_suspend_workaround and can't help you.

0 Kudos
Reply

2,285 Views
harald_krapfenb
Contributor III

Up to now, I'm not dealing with the PMIC at all; my board has no DA9053. So this code is not executed.

Involved parts are imho DDR RAM and M4IF.

0 Kudos
Reply

2,285 Views
VincentChen
Contributor I

static void loco_suspend_enter(void)
{
    if (!board_is_mx53_loco_mc34708()) {
        loco_da9053_irq_wakeup_only_fixup();
//vin        da9053_suspend_cmd_sw();
        da9053_suspend_cmd_hw(); //vin added 2012/4/11, because we have DA9053 on board

    }
}


int da9052_ldo_buck_set_voltage(struct regulator_dev *rdev,
                    int min_uV, int max_uV)
{
    struct da9052_regulator_priv *priv = rdev_get_drvdata(rdev);
    struct da9052_ssc_msg ssc_msg;
    int id = rdev_get_id(rdev);
    int ret;
    int ldo_volt = 0;

    /* KPIT - Below if condition is there for added setvoltage attribute
    in sysfs */
    if (0 == max_uV)
        max_uV = da9052_regulators[id].reg_const.max_uV;


    ...........
    ...........
    ...........


    switch (id) {
    case DA9052_LDO2:
        ssc_msg.data = (ssc_msg.data | DA9052_SUPPLY_VLDO2GO);
    break;
    case DA9052_LDO3:
        ssc_msg.data = (ssc_msg.data | DA9052_SUPPLY_VLDO3GO);
    break;
    case DA9052_BUCK_CORE:
        ssc_msg.data = (ssc_msg.data | DA9052_SUPPLY_VBCOREGO);
        ssc_msg.data &= 0x7f;//vin 2012/6/21, set the bit 7 to 0.
    break;
    case DA9052_BUCK_PRO:
        ssc_msg.data = (ssc_msg.data | DA9052_SUPPLY_VBPROGO);
    break;
    case DA9052_BUCK_MEM:
        ssc_msg.data = (ssc_msg.data | DA9052_SUPPLY_VBMEMGO);
    break;
    default:
        da9052_unlock(priv->da9052);
        return -EINVAL;
    }

    ............
    ............
    ............

}

Modified the above two functions, it works for me.


0 Kudos
Reply