Support for edt-ft5x06

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Support for edt-ft5x06

2,655 次查看
panli
Contributor II

Dear all,

we have got a capacitive touchscreen display (ETMV570G0BDHU) which we would like to test with our Sabreboard MCIMX7SABRE. Because the default configuration in device tree file only support resistive touch, I disabled it and add our configuration for capacitive touch. The touch driver edt-ft5x06 was installed in linux kernel through CONFIG TOUCHSCREEN_EDT_FT5X06. The linux kernel was built with a yocto system. The kernel version is 4.12.

After booting, we saw that the driver is connected with the device. However, touch doesn't work. We didn't see any interrupt coming from display if we press on the screen. 

Do you have any working example of device tree file for capacitive touch on this board?

best regards

Pan

标签 (1)
标记 (3)
0 项奖励
回复
1 回复

2,452 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Pan

FT5X is supported on some third party boards, for example imx6qdl-sabrelite.dtsi

linux-imx6/imx6qdl-sabrelite.dtsi at boundary-imx_4.9.x_2.0.0_ga · boundarydevices/linux-imx6 · GitH... 

linux-imx6/imx6ul-tx6ul.dtsi at boundary-imx_4.9.x_2.0.0_ga · boundarydevices/linux-imx6 · GitHub 

Sabrelite: New FT5x06 touch screen and swapped Y (input_set_abs_params) 

[RFC,1/3] ARM: dts: imx7d: add imx7d-phyboard-zeta - Patchwork 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复