Stuck at kernel startup

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Stuck at kernel startup

ソリューションへジャンプ
8,448件の閲覧回数
kat61545
Contributor II

Hello,

I have a problem when i start L4.1.15 version with rootfs files like: core-image-base, fsl-image-gui, fsl-image-qt5,...

I'm using mfgtool for imx6s

Log:

U-Boot 2016.03-svn351 (Jan 25 2019 - 10:14:46 +0800)

CPU: Freescale i.MX6DL rev1.3 at 792MHz
CPU: Commercial temperature grade (0C to 95C) at 58C
Reset cause: POR
Board: MYZR i.MX6 Evaluation Kit
Model: MY-IMX6-EK200-6S-512M
I2C: ready
DRAM: 512 MiB
MMC: FSL_SDHC: 0, FSL_SDHC: 1
SF: Detected SST25VF016B with page size 256 Bytes, erase size 64 KiB, total 2 MiB
*** Warning - bad CRC, using default environment

In: serial
Out: serial
Err: serial
delay.
delay.
delay.
config_ipu_lvds_clk: freq = 448000000.
config_ipu_lvds_clk: set pll2_pfd0 clock to 450MHz, divider = 21.
Net: Board Net Initialization Failed
No ethernet found.
Normal Boot
Hit any key to stop autoboot: 0
reading my_environment.scr
2358 bytes read in 13 ms (176.8 KiB/s)
## Executing script at 12000000
Saving Environment to SPI Flash...
SF: Detected SST25VF016B with page size 256 Bytes, erase size 64 KiB, total 2 MiB
Erasing SPI flash...Writing to SPI flash...done
Info: Linux-4.1.15 MYIMXA9 eMMC
reading myimx6ek200-6s-512m.dtb
42351 bytes read in 18 ms (2.2 MiB/s)
reading zImage-myimx6a9
7258976 bytes read in 200 ms (34.6 MiB/s)
Kernel image @ 0x12000000 [ 0x000000 - 0x6ec360 ]
## Flattened Device Tree blob at 18000000
Booting using the fdt blob at 0x18000000
Using Device Tree in place at 18000000, end 1800d56e
Using machid 0x1408 from environment

Starting kernel ...

Booting Linux on physical CPU 0x0
Linux version 4.1.15-myimx6-gd408fb6 (myzr@u12045) (gcc version 5.3.1 20160113 (Linaro GCC 5.3-2016.02) ) #1 SMP PREEMPT Fri Nov 1 13:46:05 CST 2019
CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c53c7d
CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
Machine model: MYZR i.MX6 Evaluation Kit (MY-IMX6-EK200-6S-512M)
Reserved memory: created CMA memory pool at 0x1c000000, size 320 MiB
Reserved memory: initialized node linux,cma, compatible id shared-dma-pool
Memory policy: Data cache writealloc
PERCPU: Embedded 12 pages/cpu @8bb20000 s16960 r8192 d24000 u49152
Built 1 zonelists in Zone order, mobility grouping on. Total pages: 130048
Kernel command line: console=ttymxc0,115200 nosmp root=/dev/mmcblk3p2 rootwait rw video=mxcfb0:dev=ldb,if=RGB666 ldb=sin1
PID hash table entries: 2048 (order: 1, 8192 bytes)
Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)
Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)
Memory: 177436K/524288K available (9125K kernel code, 460K rwdata, 3228K rodata, 452K init, 452K bss, 19172K reserved, 327680K cma-reserved, 0K highmem)
Virtual kernel memory layout:
vector : 0xffff0000 - 0xffff1000 ( 4 kB)
fixmap : 0xffc00000 - 0xfff00000 (3072 kB)
vmalloc : 0xa0800000 - 0xff000000 (1512 MB)
lowmem : 0x80000000 - 0xa0000000 ( 512 MB)
pkmap : 0x7fe00000 - 0x80000000 ( 2 MB)
modules : 0x7f000000 - 0x7fe00000 ( 14 MB)
.text : 0x80008000 - 0x80c18a20 (12355 kB)
.init : 0x80c19000 - 0x80c8a000 ( 452 kB)
.data : 0x80c8a000 - 0x80cfd1c0 ( 461 kB)
.bss : 0x80d00000 - 0x80d71008 ( 453 kB)
SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=2, Nodes=1
Preemptible hierarchical RCU implementation.
Additional per-CPU info printed with stalls.
RCU restricting CPUs from NR_CPUS=4 to nr_cpu_ids=2.
RCU: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=2
NR_IRQS:16 nr_irqs:16 16
L2C-310 erratum 769419 enabled
L2C-310 enabling early BRESP for Cortex-A9
L2C-310 full line of zeros enabled for Cortex-A9
L2C-310 ID prefetch enabled, offset 16 lines
L2C-310 dynamic clock gating enabled, standby mode enabled
L2C-310 cache controller enabled, 16 ways, 512 kB
L2C-310: CACHE_ID 0x410000c8, AUX_CTRL 0x76450001
ccm: ldb_di_sel already changed from reset value
ccm: ldb_di_sel workaround only for top mux
mxc_clocksource_init 3000000
Switching to timer-based delay loop, resolution 333ns
sched_clock: 32 bits at 3000kHz, resolution 333ns, wraps every 715827882841ns
clocksource mxc_timer1: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 637086815595 ns
Console: colour dummy device 80x30
Calibrating delay loop (skipped), value calculated using timer frequency.. 6.00 BogoMIPS (lpj=30000)
pid_max: default: 32768 minimum: 301
Mount-cache hash table entries: 1024 (order: 0, 4096 bytes)
Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes)
CPU: Testing write buffer coherency: ok
CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
Setting up static identity map for 0x10008280 - 0x100082d8
Brought up 1 CPUs
SMP: Total of 1 processors activated (6.00 BogoMIPS).
CPU: All CPU(s) started in SVC mode.
devtmpfs: initialized
VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4
clocksource jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
pinctrl core: initialized pinctrl subsystem
NET: Registered protocol family 16
DMA: preallocated 256 KiB pool for atomic coherent allocations
cpuidle: using governor ladder
cpuidle: using governor menu
CPU identified as i.MX6DL, silicon rev 1.3
hw-breakpoint: found 5 (+1 reserved) breakpoint and 1 watchpoint registers.
hw-breakpoint: maximum watchpoint size is 4 bytes.
imx6dl-pinctrl 20e0000.iomuxc: initialized IMX pinctrl driver
mxs-dma 110000.dma-apbh: initialized
vgaarb: loaded
SCSI subsystem initialized
usbcore: registered new interface driver usbfs
usbcore: registered new interface driver hub
usbcore: registered new device driver usb
2000000.aips-bus:usbphy_nop1 supply vcc not found, using dummy regulator
2000000.aips-bus:usbphy_nop2 supply vcc not found, using dummy regulator
i2c i2c-0: IMX I2C adapter registered
i2c i2c-0: can't use DMA
i2c i2c-1: IMX I2C adapter registered
i2c i2c-1: can't use DMA
i2c i2c-2: IMX I2C adapter registered
i2c i2c-2: can't use DMA
Linux video capture interface: v2.00
pps_core: LinuxPPS API ver. 1 registered
pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <[email protected]>
PTP clock support registered
imx-ipuv3 2400000.ipu: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)
mxc_mipi_csi2 21dc000.mipi_csi: i.MX MIPI CSI2 driver probed
mxc_mipi_csi2 21dc000.mipi_csi: i.MX MIPI CSI2 dphy version is 0x3130302a
MIPI CSI2 driver module loaded
Advanced Linux Sound Architecture Driver Initialized.
Bluetooth: Core ver 2.20
NET: Registered protocol family 31
Bluetooth: HCI device and connection manager initialized
Bluetooth: HCI socket layer initialized
Bluetooth: L2CAP socket layer initialized
Bluetooth: SCO socket layer initialized
Switched to clocksource mxc_timer1
NET: Registered protocol family 2
TCP established hash table entries: 4096 (order: 2, 16384 bytes)
TCP bind hash table entries: 4096 (order: 3, 32768 bytes)
TCP: Hash tables configured (established 4096 bind 4096)
UDP hash table entries: 256 (order: 1, 8192 bytes)
UDP-Lite hash table entries: 256 (order: 1, 8192 bytes)
NET: Registered protocol family 1
RPC: Registered named UNIX socket transport module.
RPC: Registered udp transport module.
RPC: Registered tcp transport module.
RPC: Registered tcp NFSv4.1 backchannel transport module.
CPU PMU: Failed to parse /soc/pmu/interrupt-affinity[0]
hw perfevents: enabled with armv7_cortex_a9 PMU driver, 7 counters available
imx rpmsg driver is registered.
Bus freq driver module loaded
futex hash table entries: 512 (order: 3, 32768 bytes)
VFS: Disk quotas dquot_6.6.0
VFS: Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
NFS: Registering the id_resolver key type
Key type id_resolver registered
Key type id_legacy registered
jffs2: version 2.2. (NAND) © 2001-2006 Red Hat, Inc.
fuse init (API version 7.23)
io scheduler noop registered
io scheduler deadline registered
io scheduler cfq registered (default)
imx-weim 21b8000.weim: Driver registered.
backlight supply power not found, using dummy regulator
MIPI DSI driver module loaded
MIPI DSI driver module loaded
20e0000.hdmi_video supply HDMI not found, using dummy regulator
mxc_sdc_fb fb@0: registered mxc display driver ldb
imx-ipuv3 2400000.ipu: IPU DMFC DP HIGH RESOLUTION: 1(0,1), 5B(2~5), 5F(6,7)
Console: switching to colour frame buffer device 128x37
mxc_hdmi 20e0000.hdmi_video: Detected HDMI controller 0x13:0x1a:0xa0:0xc1
fbcvt: 1920x1080@60: CVT Name - 2.073M9
mxc_sdc_fb fb@1: registered mxc display driver hdmi
imx-sdma 20ec000.sdma: no iram assigned, using external mem
imx-sdma 20ec000.sdma: no event needs to be remapped
imx-sdma 20ec000.sdma: loaded firmware 3.3
imx-sdma 20ec000.sdma: initialized
2020000.serial: ttymxc0 at MMIO 0x2020000 (irq = 26, base_baud = 5000000) is a IMX
console [ttymxc0] enabled
21e8000.serial: ttymxc1 at MMIO 0x21e8000 (irq = 302, base_baud = 5000000) is a IMX
21ec000.serial: ttymxc2 at MMIO 0x21ec000 (irq = 303, base_baud = 5000000) is a IMX
21f0000.serial: ttymxc3 at MMIO 0x21f0000 (irq = 304, base_baud = 5000000) is a IMX
21f4000.serial: ttymxc4 at MMIO 0x21f4000 (irq = 305, base_baud = 5000000) is a IMX
imx sema4 driver is registered.
[drm] Initialized drm 1.1.0 20060810
[drm] Initialized vivante 1.0.0 20120216 on minor 0
brd: module loaded
loop: module loaded
m25p80 spi0.0: sst25vf016b (2048 Kbytes)
spi_imx 2008000.ecspi: probed
spi_imx 200c000.ecspi: probed
CAN device driver interface
2090000.flexcan supply xceiver not found, using dummy regulator
flexcan 2090000.flexcan: device registered (reg_base=a0a50000, irq=32)
2094000.flexcan supply xceiver not found, using dummy regulator
flexcan 2094000.flexcan: device registered (reg_base=a0a58000, irq=33)
2188000.ethernet supply phy not found, using dummy regulator
pps pps0: new PPS source ptp0
libphy: fec_enet_mii_bus: probed
fec 2188000.ethernet eth0: registered PHC device 0
Intel(R) Wireless WiFi driver for Linux
Copyright(c) 2003- 2015 Intel Corporation
iwl4965: Intel(R) Wireless WiFi 4965 driver for Linux, in-tree:
iwl4965: Copyright(c) 2003-2011 Intel Corporation
usbcore: registered new interface driver asix
usbcore: registered new interface driver ax88179_178a
usbcore: registered new interface driver cdc_ether
usbcore: registered new interface driver smsc95xx
usbcore: registered new interface driver net1080
usbcore: registered new interface driver cdc_subset
usbcore: registered new interface driver zaurus
usbcore: registered new interface driver cdc_ncm
GobiNet: Quectel_WCDMA&LTE_Linux&Android_GobiNet_Driver_V1.3.0
usbcore: registered new interface driver GobiNet
ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
ehci-pci: EHCI PCI platform driver
ehci-mxc: Freescale On-Chip EHCI Host driver
usbcore: registered new interface driver usb-storage
usbcore: registered new interface driver usbserial
usbcore: registered new interface driver usbserial_generic
usbserial: USB Serial support registered for generic
usbcore: registered new interface driver option
usbserial: USB Serial support registered for GSM modem (1-port)
usbcore: registered new interface driver usb_ehset_test
2184800.usbmisc supply vbus-wakeup not found, using dummy regulator
ci_hdrc ci_hdrc.1: EHCI Host Controller
ci_hdrc ci_hdrc.1: new USB bus registered, assigned bus number 1
ci_hdrc ci_hdrc.1: USB 2.0 started, EHCI 1.00
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
mousedev: PS/2 mouse device common for all mice
myts_ft5x0x 2-0038: touchscreen probe failed
myts_ft5x0x: probe of 2-0038 failed with error -5
snvs_rtc 20cc000.snvs:snvs-rtc-lp: rtc core: registered 20cc000.snvs:snvs-r as rtc0
i2c /dev entries driver
IR NEC protocol handler initialized
IR RC5(x/sz) protocol handler initialized
IR RC6 protocol handler initialized
IR JVC protocol handler initialized
IR Sony protocol handler initialized
IR SANYO protocol handler initialized
IR Sharp protocol handler initialized
IR MCE Keyboard/mouse protocol handler initialized
IR XMP protocol handler initialized
mxc_v4l2_output v4l2_out: V4L2 device registered as video16
mxc_v4l2_output v4l2_out: V4L2 device registered as video17
mxc_v4l2_output v4l2_out: V4L2 device registered as video18
imx2-wdt 20bc000.wdog: use WDOG_B to reboot.
imx2-wdt 20bc000.wdog: timeout 60 sec (nowayout=0)
Bluetooth: HCI UART driver ver 2.3
Bluetooth: HCI UART protocol H4 registered
Bluetooth: HCI UART protocol BCSP registered
Bluetooth: HCI UART protocol ATH3K registered
usbcore: registered new interface driver bcm203x
usbcore: registered new interface driver btusb
usbcore: registered new interface driver ath3k
sdhci: Secure Digital Host Controller Interface driver
sdhci: Copyright(c) Pierre Ossman
sdhci-pltfm: SDHCI platform and OF driver helper
/soc/aips-bus@02100000/usdhc@02198000: voltage-ranges unspecified
sdhci-esdhc-imx 2198000.usdhc: Got CD GPIO
sdhci-esdhc-imx 2198000.usdhc: Got WP GPIO
sdhci-esdhc-imx 2198000.usdhc: No vmmc regulator found
sdhci-esdhc-imx 2198000.usdhc: No vqmmc regulator found
mmc2: SDHCI controller on 2198000.usdhc [2198000.usdhc] using ADMA
/soc/aips-bus@02100000/usdhc@0219c000: voltage-ranges unspecified
sdhci-esdhc-imx 219c000.usdhc: No vmmc regulator found
sdhci-esdhc-imx 219c000.usdhc: No vqmmc regulator found
mmc3: SDHCI controller on 219c000.usdhc [219c000.usdhc] using ADMA
mxc_vpu 2040000.vpu_fsl: VPU initialized
mxc_vdoa 21e4000.vdoa: i.MX Video Data Order Adapter(VDOA) driver probed
mxc_hdmi_cec soc:hdmi_cec@00120000: HDMI CEC initialized
galcore: clk_get vg clock failed, disable vg!
Galcore version 5.0.11.41671
mmc3: MAN_BKOPS_EN bit is not set
mmc3: new DDR MMC card at address 0001
mmcblk3: mmc3:0001 Q2J54A 3.64 GiB
mmcblk3boot0: mmc3:0001 Q2J54A partition 1 2.00 MiB
mmcblk3boot1: mmc3:0001 Q2J54A partition 2 2.00 MiB
mmcblk3rpmb: mmc3:0001 Q2J54A partition 3 512 KiB
mmcblk3: p1 p2
caam 2100000.caam: Entropy delay = 3200
caam 2100000.caam: Instantiated RNG4 SH0
caam 2100000.caam: Instantiated RNG4 SH1
caam 2100000.caam: device ID = 0x0a16010000000100 (Era -524)
caam 2100000.caam: job rings = 2, qi = 0
caam algorithms registered in /proc/crypto
caam_jr 2101000.jr0: registering rng-caam
platform caam_sm: blkkey_ex: 4 keystore units available
platform caam_sm: 64-bit clear key:
platform caam_sm: [0000] 00 01 02 03 04 0f 06 07
platform caam_sm: 64-bit black key:
platform caam_sm: [0000] 44 87 d8 7d 0a 27 6c 35
platform caam_sm: [0008] 50 75 8c 22 64 f6 04 9a
platform caam_sm: 128-bit clear key:
platform caam_sm: [0000] 00 01 02 03 04 0f 06 07
platform caam_sm: [0008] 08 09 0a 0b 0c 0d 0e 0f
platform caam_sm: 128-bit black key:
platform caam_sm: [0000] 70 1b 69 1f 73 fa ee 08
platform caam_sm: [0008] ea 34 95 16 03 86 30 42
platform caam_sm: 192-bit clear key:
platform caam_sm: [0000] 00 01 02 03 04 0f 06 07
platform caam_sm: [0008] 08 09 0a 0b 0c 0d 0e 0f
platform caam_sm: [0016] 10 11 12 13 14 15 16 17
platform caam_sm: 192-bit black key:
platform caam_sm: [0000] c2 37 91 65 90 ba 75 b7
platform caam_sm: [0008] 4c 97 9e ef 47 9d 18 64
platform caam_sm: [0016] fd 75 1a 4d 57 23 59 81
platform caam_sm: [0024] 9c ff 22 f1 15 43 f6 1e
platform caam_sm: 256-bit clear key:
platform caam_sm: [0000] 00 01 02 03 04 0f 06 07
platform caam_sm: [0008] 08 09 0a 0b 0c 0d 0e 0f
platform caam_sm: [0016] 10 11 12 13 14 15 16 17
platform caam_sm: [0024] 18 19 1a 1b 1c 1d 1e 1f
platform caam_sm: 256-bit black key:
platform caam_sm: [0000] b2 fe a7 f7 db d8 2e f4
platform caam_sm: [0008] 83 80 c8 ed e1 52 0f 6e
platform caam_sm: [0016] 7a 19 dd b6 e8 86 8b 03
platform caam_sm: [0024] ec cf f9 cd 62 16 4f b2
platform caam_sm: 64-bit unwritten blob:
platform caam_sm: [0000] 00 00 00 00 00 00 00 00
platform caam_sm: [0008] 00 00 00 00 00 00 00 00
platform caam_sm: [0016] 00 00 00 00 00 00 00 00
platform caam_sm: [0024] 00 00 00 00 00 00 00 00
platform caam_sm: [0032] 00 00 00 00 00 00 00 00
platform caam_sm: [0040] 00 00 00 00 00 00 00 00
platform caam_sm: [0048] 00 00 00 00 00 00 00 00
platform caam_sm: [0056] 00 00 00 00 00 00 00 00
platform caam_sm: [0064] 00 00 00 00 00 00 00 00
platform caam_sm: [0072] 00 00 00 00 00 00 00 00
platform caam_sm: [0080] 00 00 00 00 00 00 00 00
platform caam_sm: [0088] 00 00 00 00 00 00 00 00
platform caam_sm: 128-bit unwritten blob:
platform caam_sm: [0000] 00 00 00 00 00 00 00 00
platform caam_sm: [0008] 00 00 00 00 00 00 00 00
platform caam_sm: [0016] 00 00 00 00 00 00 00 00
platform caam_sm: [0024] 00 00 00 00 00 00 00 00
platform caam_sm: [0032] 00 00 00 00 00 00 00 00
platform caam_sm: [0040] 00 00 00 00 00 00 00 00
platform caam_sm: [0048] 00 00 00 00 00 00 00 00
platform caam_sm: [0056] 00 00 00 00 00 00 00 00
platform caam_sm: [0064] 00 00 00 00 00 00 00 00
platform caam_sm: [0072] 00 00 00 00 00 00 00 00
platform caam_sm: [0080] 00 00 00 00 00 00 00 00
platform caam_sm: [0088] 00 00 00 00 00 00 00 00
platform caam_sm: 196-bit unwritten blob:
platform caam_sm: [0000] 00 00 00 00 00 00 00 00
platform caam_sm: [0008] 00 00 00 00 00 00 00 00
platform caam_sm: [0016] 00 00 00 00 00 00 00 00
platform caam_sm: [0024] 00 00 00 00 00 00 00 00
platform caam_sm: [0032] 00 00 00 00 00 00 00 00
platform caam_sm: [0040] 00 00 00 00 00 00 00 00
platform caam_sm: [0048] 00 00 00 00 00 00 00 00
platform caam_sm: [0056] 00 00 00 00 00 00 00 00
platform caam_sm: [0064] 00 00 00 00 00 00 00 00
platform caam_sm: [0072] 00 00 00 00 00 00 00 00
platform caam_sm: [0080] 00 00 00 00 00 00 00 00
platform caam_sm: [0088] 00 00 00 00 00 00 00 00
platform caam_sm: 256-bit unwritten blob:
platform caam_sm: [0000] 00 00 00 00 00 00 00 00
platform caam_sm: [0008] 00 00 00 00 00 00 00 00
platform caam_sm: [0016] 00 00 00 00 00 00 00 00
platform caam_sm: [0024] 00 00 00 00 00 00 00 00
platform caam_sm: [0032] 00 00 00 00 00 00 00 00
platform caam_sm: [0040] 00 00 00 00 00 00 00 00
platform caam_sm: [0048] 00 00 00 00 00 00 00 00
platform caam_sm: [0056] 00 00 00 00 00 00 00 00
platform caam_sm: [0064] 00 00 00 00 00 00 00 00
platform caam_sm: [0072] 00 00 00 00 00 00 00 00
platform caam_sm: [0080] 00 00 00 00 00 00 00 00
platform caam_sm: [0088] 00 00 00 00 00 00 00 00
platform caam_sm: 64-bit black key in blob:
platform caam_sm: [0000] db 1c bc 4b 80 1b 0f 09
platform caam_sm: [0008] f7 cd 2d b8 db f7 11 ac
platform caam_sm: [0016] b7 be 0f 88 0c d8 c1 0e
platform caam_sm: [0024] f3 48 11 3e 44 d2 89 8c
platform caam_sm: [0032] 6a 3b 23 1a 99 7f e8 15
platform caam_sm: [0040] 9f 1e 07 14 da 71 6e fc
platform caam_sm: [0048] ad c1 89 ce 09 ed 8c 46
platform caam_sm: [0056] 00 00 00 00 00 00 00 00
platform caam_sm: [0064] 00 00 00 00 00 00 00 00
platform caam_sm: [0072] 00 00 00 00 00 00 00 00
platform caam_sm: [0080] 00 00 00 00 00 00 00 00
platform caam_sm: [0088] 00 00 00 00 00 00 00 00
platform caam_sm: 128-bit black key in blob:
platform caam_sm: [0000] 59 ab b6 d9 29 0f 98 b8
platform caam_sm: [0008] 5b 14 30 9f 62 25 27 ea
platform caam_sm: [0016] 68 16 6f 7a c0 9a 10 72
platform caam_sm: [0024] 32 f3 b0 40 d2 21 9c 5f
platform caam_sm: [0032] ba 39 d7 47 16 1b 23 5e
platform caam_sm: [0040] 37 fa f7 d5 5c 22 e5 16
platform caam_sm: [0048] 0f a9 80 24 0c b4 76 44
platform caam_sm: [0056] dc d8 07 28 be 71 17 a1
platform caam_sm: [0064] 00 00 00 00 00 00 00 00
platform caam_sm: [0072] 00 00 00 00 00 00 00 00
platform caam_sm: [0080] 00 00 00 00 00 00 00 00
platform caam_sm: [0088] 00 00 00 00 00 00 00 00
platform caam_sm: 192-bit black key in blob:
platform caam_sm: [0000] f1 5e ad 61 16 c5 f3 b4
platform caam_sm: [0008] 55 fc a8 b1 79 e4 27 b2
platform caam_sm: [0016] 8a 9e d8 e3 bf cc 99 f1
platform caam_sm: [0024] ce 2d 33 f1 36 fc da 6a
platform caam_sm: [0032] 4c 99 f5 35 c2 95 bc 54
platform caam_sm: [0040] bc db cf 16 90 1a 25 cc
platform caam_sm: [0048] f9 b2 0b 93 54 2d 2b 72
platform caam_sm: [0056] 97 d9 67 97 f5 e3 eb cb
platform caam_sm: [0064] 16 15 dd 77 3d 4b 37 2e
platform caam_sm: [0072] 00 00 00 00 00 00 00 00
platform caam_sm: [0080] 00 00 00 00 00 00 00 00
platform caam_sm: [0088] 00 00 00 00 00 00 00 00
platform caam_sm: 256-bit black key in blob:
platform caam_sm: [0000] d1 8b b4 9d a7 24 2f 43
platform caam_sm: [0008] 8f 55 44 f7 7b 1e 88 e4
platform caam_sm: [0016] 57 4a 78 0e a1 36 29 38
platform caam_sm: [0024] bb 3c 6d cd 3a 39 56 7b
platform caam_sm: [0032] 15 69 6e 5e 99 23 08 0a
platform caam_sm: [0040] 4b 57 4c 68 75 b4 3e c4
platform caam_sm: [0048] e4 80 bb bb 8f 6f 6d 88
platform caam_sm: [0056] 35 c7 e9 1f 02 f4 5e a2
platform caam_sm: [0064] 5f f9 bd 34 e3 42 58 cb
platform caam_sm: [0072] f8 68 9f 89 b8 3b bf 20
platform caam_sm: [0080] 00 00 00 00 00 00 00 00
platform caam_sm: [0088] 00 00 00 00 00 00 00 00
platform caam_sm: restored 64-bit black key:
platform caam_sm: [0000] 13 5a 17 a0 77 3c f1 dd
platform caam_sm: [0008] b8 61 94 dd ec 3a 60 52
platform caam_sm: restored 128-bit black key:
platform caam_sm: [0000] 70 1b 69 1f 73 fa ee 08
platform caam_sm: [0008] ea 34 95 16 03 86 30 42
platform caam_sm: restored 192-bit black key:
platform caam_sm: [0000] c2 37 91 65 90 ba 75 b7
platform caam_sm: [0008] 4c 97 9e ef 47 9d 18 64
platform caam_sm: [0016] c6 bc dd 0d ed 4e 90 36
platform caam_sm: [0024] 9d b7 4c fc 7a a0 1d ac
platform caam_sm: restored 256-bit black key:
platform caam_sm: [0000] b2 fe a7 f7 db d8 2e f4
platform caam_sm: [0008] 83 80 c8 ed e1 52 0f 6e
platform caam_sm: [0016] 7a 19 dd b6 e8 86 8b 03
platform caam_sm: [0024] ec cf f9 cd 62 16 4f b2
usbcore: registered new interface driver usbhid
usbhid: USB HID core driver
wm8962 0-001a: Failed to read ID register
wm8962: probe of 0-001a failed with error -5
fsl-asrc 2034000.asrc: driver registered
imx-wm8962 sound: failed to find codec platform device
imx-wm8962: probe of sound failed with error -22
imx-audio-hdmi sound-hdmi: hdmi-hifi <-> soc:hdmi_audio@00120000 mapping ok
NET: Registered protocol family 26
NET: Registered protocol family 10
sit: IPv6 over IPv4 tunneling driver
NET: Registered protocol family 17
can: controller area network core (rev 20120528 abi 9)
NET: Registered protocol family 29
can: raw protocol (rev 20120528)
can: broadcast manager protocol (rev 20120528 t)
can: netlink gateway (rev 20130117) max_hops=1
Bluetooth: RFCOMM TTY layer initialized
Bluetooth: RFCOMM socket layer initialized
Bluetooth: RFCOMM ver 1.11
Bluetooth: BNEP (Ethernet Emulation) ver 1.3
Bluetooth: BNEP filters: protocol multicast
Bluetooth: BNEP socket layer initialized
Bluetooth: HIDP (Human Interface Emulation) ver 1.2
Bluetooth: HIDP socket layer initialized
8021q: 802.1Q VLAN Support v1.8
lib80211: common routines for IEEE802.11 drivers
Key type dns_resolver registered
1ffc000.pcie supply pcie-bus not found, using dummy regulator
imx6q-pcie 1ffc000.pcie: phy link never came up
imx6q-pcie 1ffc000.pcie: failed to initialize host
imx6q-pcie: probe of 1ffc000.pcie failed with error -22
imx_epdc_fb 20f4000.epdc: can't get/select pinctrl
dhd_module_init in
input: gpio-keys as /devices/soc0/gpio-keys/input/input1
snvs_rtc 20cc000.snvs:snvs-rtc-lp: setting system clock to 1970-01-01 00:00:00 UTC (0)
wm8962-supply: disabling
usb_otg_vbus: disabling
ALSA device list:
#0: imx-hdmi-soc
EXT3-fs (mmcblk3p2): error: couldn't mount because of unsupported optional features (240)
EXT2-fs (mmcblk3p2): error: couldn't mount because of unsupported optional features (240)
EXT4-fs (mmcblk3p2): mounted filesystem with ordered data mode. Opts: (null)
VFS: Mounted root (ext4 filesystem) on device 179:2.
devtmpfs: mounted
Freeing unused kernel memory: 452K (80c19000 - 80c8a000)
INIT: version 2.88 booting
Starting udev
udevd[179]: starting version 3.1.5
random: udevd urandom read with 12 bits of entropy available
ov564x 0-003c: no sensor reset pin available
ov564x: probe of 0-003c failed with error -22
1-003c supply DOVDD not found, using dummy regulator
1-003c supply DVDD not found, using dummy regulator
1-003c supply AVDD not found, using dummy regulator
0-003c supply DOVDD not found, using dummy regulator
0-003c supply DVDD not found, using dummy regulator
ERROR: v4l2 capture: slave not found!
ERROR: v4l2 capture: slave not found!
0-003c supply AVDD not found, using dummy regulator
ov5642_read_reg:write reg error:reg=300a
camera ov5642 is not found
ov5640_read_reg:write reg error:reg=300a
camera ov5640_mipi is not found
EXT4-fs (mmcblk3p2): re-mounted. Opts: data=ordered
bootlogd: cannot allocate pseudo tty: No such file or directory
Populating dev cache
ALSA: Restoring mixer settings...
Tue Sep 25 17:39:07 UTC 2018
random: nonblocking pool is initialized

ラベル(3)
タグ(4)
0 件の賞賛
返信
1 解決策
8,321件の閲覧回数
kat61545
Contributor II

Thank for reply, igorpadykov

I found the solution in topic:https://community.nxp.com/thread/455104 

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
8,321件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Oliver

hanging may be caused by memory, so recommended to run ddr test

i.MX 6/7 DDR Stress Test Tool  

update uboot dcd header

mx6solo_4x_mt41j128.cfg\mx6sabresd\freescale\board - uboot-imx - i.MX U-Boot 

and rebuild mfg tool firmware, recipes used to build a manufacturing tool image are
linux-imx-mfgtool and u-boot-mfgtool.

Also one can consider sb_loader

Imx usb loader - Variscite Wiki 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
8,322件の閲覧回数
kat61545
Contributor II

Thank for reply, igorpadykov

I found the solution in topic:https://community.nxp.com/thread/455104 

0 件の賞賛
返信