Strange MMC boot behavior

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Strange MMC boot behavior

1,020 次查看
robertwood
Contributor I
  1. On our iMX6DL board we have a Micron MTFC4GACAJCN-4M IT, eMMC device on uSDHC3, which is DDR and byte capable. When configuring for boot, we find the processor boots when the CONFIG2(7:5) field is set to "111" or "010" but not to "110".  Now the reference manual states in Table 5-6

Bus Width:

000 - 1-bit

001 - 4-bit

010 - 8-bit

101 - 4-bit

DDR (MMC 4.4)

110 - 8-bit DDR (MMC 4.4)

Else - Reserved

What are we doing wrong or right :smileywink:

0 项奖励
回复
1 回复

879 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  Please try to check Your boot configuration via SRC Boot Mode Register 2 (SRC_SBMR2),

which contains bits that reflect the status of Boot Mode Pins. It may be taken from
report of i.MX6/7 DDR Stress Test Tool V2.52

The Stress Test should be run just after boot failure.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复