Sticky Bit error of i.MX6Solo with using debugger

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Sticky Bit error of i.MX6Solo with using debugger

ソリューションへジャンプ
1,601件の閲覧回数
yuuki
Senior Contributor II

Dear All,

In our original board, we accessed the EIM_CS0 area(0x0800_0000-) by using JTAG.

However, when we access the EIM_CS0 area after a system Boot from SD, Sticky Bit error occurs.
Word access and double word access were tried, but it was the same result.

May I have any advice to evade this error?


Best Regards,
Yuuki

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 解決策
1,468件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Yuuki

had you set CCM_CGPR6, CG5 for EIM clock enabling ?

Best regards

igor

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,469件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Yuuki

had you set CCM_CGPR6, CG5 for EIM clock enabling ?

Best regards

igor

0 件の賞賛
返信
1,468件の閲覧回数
yuuki
Senior Contributor II

Dear igor-san,

Thank you very much for your support.

I found CG5 field of the CCM_CCGR6 register having been 00.

The problem was solved by setting this value to "11".

Best Regards,

Yuuki

0 件の賞賛
返信