Steps to connect a microcontroller to imx8mp using a usb cdc class

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Steps to connect a microcontroller to imx8mp using a usb cdc class

720 次查看
ababatola
Contributor III

Hi,

For my project, I am meant to send data to my imx8mp device from the usb port of a microcontroller.  This is a completely new topic for me and I would like to know if nxp have some material in this light.  

Below are some information to my project

1.  IMX8 is the host device and would fetch data from the microcontoller when it needs the data.  

2.  There is a 2 port USB hub between the imx8 and the microcontroller.

3. I have selected the usb cdc class for my usb operation and high speed.

4. I would like to use the libusb library.

5.  I also want to write a linux user space app?

6.  I would also write a c# application to receive data from the imx8mp

Are there any NXP application report or link or previous issues that can help me in this

Thanks.

标签 (1)
0 项奖励
回复
1 回复

695 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

All the previous question work with linux BSP, so please download, we have no an application ready but you can download someone for it.

https://www.nxp.com/design/design-center/software/embedded-software/i-mx-software/embedded-linux-for...

 

Regards

 

0 项奖励
回复