Steps to add python packages into yocto build

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Steps to add python packages into yocto build

5,482件の閲覧回数
krsuresh
Contributor III

Hi Team,

We would appreciate it if you could tell me how to build a core-minimal-image with following python packages,
   

tflite-support
tensorstore
tflite-support-nightly
tensorflow-addons

 

Thanks,
Sureshkumar R

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

5,453件の閲覧回数
Dhruvit
NXP TechSupport
NXP TechSupport

Hi @krsuresh,

I hope you are doing well.

To add the above packes in the yocto build, one needs to have a bitbake recipe for the same.

NXP Yocto BSP doesn't contain recipes for the same.

Customer needs to create their own bitbake recipes to add above packages.

One can refer to various recipes at meta-imx/meta-ml/recipes-libraries
/tensorflow-lite/

Thanks & Regards,
Dhruvit Vasavada

0 件の賞賛
返信

5,449件の閲覧回数
krsuresh
Contributor III

Hi @Dhruvit 

 

Thanks for the reply.

I will check the recipes. Thanks for the information.

 

Thanks & Regards,

Sureshkumar R

 

0 件の賞賛
返信