Startup problem from h/w reset

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Startup problem from h/w reset

1,764件の閲覧回数
roybunce
Contributor II

Hi all,

I've designed a module based on the QSB, with a Ripley PMIC but otherwise generally following the original QSB schematic. (The Ripley version wasn't available when I did the schematic.) I'm booting from SD and when it boots everything seems perfect; u-boot runs, Linux loads and runs from the SD, a memory test passes, the display, ethernet and USB are OK and all the relevant tests in the "unit_tests" directory pass.

The problem is that most of the time it fails to boot. Repeated on/off cycles will eventually get it going, but usually it just crashes with no output on the serial port and no response to serial commands.

It must be a hardware problem, because the same SD card always boots correctly on the QSB but I'm struggling to work out why. The power rails, clock and reset seem OK, and when it does boot there are no signs of anything flaky. Has anyone seen a similar problem, or have any ideas what might be going wrong?

Regards,

Roy

ラベル(1)
0 件の賞賛
返信
1 返信

1,610件の閲覧回数
roybunce
Contributor II

SOLVED!!

It was a software problem in u-boot. One clue was that eboot always started correctly.

The answer was posted in another thread ( http://imxcommunity.org/forum/topics/imx53qsb-boot-up-problems ) by Jerry Fan. Adding the line "REG_LD_AND_STR_OP(29, 0x0f8, 0x00000800)" in flash_header.S forces a delay line measurement in the SDRAM controller. Thanks Jerry!

0 件の賞賛
返信