Standalone program to test Ethernet in I.MX28 using internal RAM

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Standalone program to test Ethernet in I.MX28 using internal RAM

1,277 次查看
Ramtry
Contributor III

Hi,

 

I am trying to test Ethernet using standalone program without using any OS. I designed a new board based on I.MX28EVK and want to test ethernet. I tried ODBS to test the Ethernet and it works fine but it using ddr2. So, I just added Ethernet driver files from ODBS to my standalone program and when i am trying to test, it showing error as follows

 

ENET0<->ENET1 loopback test

Please make sure cross-switch Ethernet cable (typically red) is present

FEC LAN8720 PHY: ID=x

enet phy status 0: 782d

FEC 0: [ FULL_DUPLEX ] [ connected ] [ 100M bps ]

ENET link status check PASS

send packet Enet0->Enet1

enet0 tx ok

enet1 rx fail

Ethernet Failed

cycle pass

 

I attached the program for your reference. I don't know what am missing while adding Ethernet driver file to my standalone program. Can anyone please give suggestion to solve this problem.

Original Attachment has been moved to: Ethernet_test.rar

标记 (4)
0 项奖励
回复
1 回复

917 次查看
alejandrolozan1
NXP Employee
NXP Employee

Hi,

Have you tried to migrate or test the entire obds in your board?

If so and it works, I would take a look at the clock settings first.

I wonder if you are able debug to start narrowing down the difference between projects.

You may want to try to add your application to the obds, just to make sure that the problem is not at application level.

Best Regards,

Alejandro

0 项奖励
回复