To use external clock with spread spectrum for i.MX6 IPU/LDB.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

To use external clock with spread spectrum for i.MX6 IPU/LDB.

跳至解决方案
1,996 次查看
satoshishimoda
Senior Contributor I

Hi community,

I want to confirm the specification of i.MX6 PLL in CCM module.

Actually, I want to use a external clock with spread spectrum via CLK1_N/CLK1_P pin to IPU, LDB as following route.

external clock -> CLK1_N, CLK1_P -> PLL5(CCM_ANALOG) -> CCM -> IPU, LDB

In this case, I think spread spectrum is preserve if I set PLL5 to bypass mode by BYPASS bit (CCM_ANALOG_PLL_VIDEOn[16] in chapter18.7.11 of IMX6DQRM Rev.1).

Is this correct?

Or spread spectrum will be cancelled by PLL5 even if it is set to bypass mode?

Best Regards,

Satoshi Shimoda

标签 (4)
标记 (2)
0 项奖励
回复
1 解答
1,237 次查看
alejandrolozan1
NXP Employee
NXP Employee

Hi,

As per the RM the System PLL or PLL2 is the one that features spread spectrum.

And it is different to the video PLL or PLL5. Therefore the spread spectrum should be preserved in case you want to bypass the PLL5.

Best Regards,

Alejandro

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,238 次查看
alejandrolozan1
NXP Employee
NXP Employee

Hi,

As per the RM the System PLL or PLL2 is the one that features spread spectrum.

And it is different to the video PLL or PLL5. Therefore the spread spectrum should be preserved in case you want to bypass the PLL5.

Best Regards,

Alejandro

0 项奖励
回复