Standalone application in u-boot

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Standalone application in u-boot

跳至解决方案
1,678 次查看
rans
Senior Contributor I

Hello,

I am trying to load standalone application.
It works fine with the hello_world example ( bin format).
Then I move to build and run another application (uc/os) in eclipse.
The problem is that the bin format is very large.
Is there a way to load a standalone application in another format ?

Regards,
Ran

0 项奖励
回复
1 解答
1,445 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Ran

bin format is standard format, probably one can use some

kind of compression, but seems it will require customization.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
3 回复数
1,446 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Ran

bin format is standard format, probably one can use some

kind of compression, but seems it will require customization.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
1,445 次查看
rans
Senior Contributor I

Hi Igor,

Thanks for reply.

Is it possible to load image format (elf converted with mkimage) ?

Thanks.

Ran

0 项奖励
回复
1,445 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Ran

for uboot proper way to post it on uboot mail list

U-Boot Info Page 

Best regards
igor

0 项奖励
回复