Srart custom device based on imx8qxp

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Srart custom device based on imx8qxp

1,381 Views
cupol2990
Contributor I

Hello. Our team developed custom device based on imx8qxp mcu. We have only emmc (no SD card). Now we try to start processor in serial download mode to flashing emmc. We use usb otg 2 and uart2 through ftdi for connection to PC, but we are getting error "unknown usb device" on windows 10 host. PC cannot get device descriptor. Whether imx8qxp has default usb downloader from box or not? If not, what we must do to start it (connect jtag or other)? We have imx8mmevk. It works fine.

Tags (1)
0 Kudos
Reply
4 Replies

1,362 Views
cupol2990
Contributor I

Ok, we've probably found problem. We didn't connect usbotg1 vbus to 5V, which is required for bootmode. We leaved it floating despite imx specification. 

So, we have another question. Can we use cortex m4 to flash emmc via jtag?

0 Kudos
Reply

1,359 Views
riteshmpatel
NXP TechSupport
NXP TechSupport

Hi @cupol2990,

I hope you are doing well.

Happy to know that the issue has been resolved.

I don't think it is not possible to flash eMMC via JTAG through M4 core since M4 SDK does not have driver for uSDHC.

Thanks & Regards,
Ritesh M Patel

 

0 Kudos
Reply

1,348 Views
cupol2990
Contributor I

Thanks for your answer.

We have also quad spi flash on the board. It has 32 mb size. We want to flash quad spi only u-boot without linux using another device, not cortex m4. Then using u-boot from quad spi we will flash linux image to emmc on board. Is it possible? 

0 Kudos
Reply

1,346 Views
riteshmpatel
NXP TechSupport
NXP TechSupport

Hi @cupol2990,

I request you to please raise a new ticket with your other query.

Thanks & Regards,
Ritesh M Patel

0 Kudos
Reply