Spreadspectrum for HDMI

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Spreadspectrum for HDMI

4,396 Views
sudarkb
Contributor II

I have some doubts regarding the HDMI clock sources and enabling spreadspectrum for HDMI. I am working on a custom board which has IMX6Quad. I have listed my questions below.

1) Can we enable spreadspectrum for HDMI interface? If yes, How should we enable spreadspectrum for HDMI. Is it the similar process as done for LVDS/LCD interface, where the parent clock is changed to PLL2_PFD2 for the IPU1_DI0 interface and enabling SS in PLL2?

2) I understand that there is VIDEO_27M clock source which is used to generate the TMDS signal from HDMI_PHY and it seems the IPU output is given to HDMI TX controller. How are these two clocks interlinked? will enabling SS in IPU output gets reflected on TMDS signals?

Thanks,
Sudar.K.B.

0 Kudos
Reply
3 Replies

3,867 Views
igorpadykov
NXP Employee
NXP Employee

Hi Sudar

you are right that spread spectrum should be provided by phy,

but I am afraid that i.MX6Q hdmi phy is not able to produce spread spectrum

clock, opposite to sata or pcie, where such descriptions can be found in reference manual.

For emi issues one can slightly  tweak HDMI preemph and termination values,
described in sect.2 "Software configuration and procedures"
AN4671 (rev.0,  4/2013) "i.MX 6 Series HDMI Test Method for
Eye Pattern and Electrical Characteristics" and
Table 34-13 "Driver Voltage Level", Table 34-6 "Single-Ended Source
Termination Resistance Settings" i.MX6DQ Reference Manual

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

3,867 Views
alexandersamuti
Contributor I

But what about this documents - https://community.nxp.com/docs/DOC-100036 ?

0 Kudos
Reply

3,867 Views
igorpadykov
NXP Employee
NXP Employee

this document is about pll2 spread spectrum, not hdmi phy pll.

0 Kudos
Reply