Specifying display framebuffer characteristics on kernel command line

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Specifying display framebuffer characteristics on kernel command line

1,675件の閲覧回数
admin
Specialist II

Saved FAQ from Freescale.com for information only:

Topic: Display, Bootup

 

Question.  The framebuffer bit depth can be set after Ubuntu has started, by using the fbset utility on the command line. If one wants a bit depth, resolution, or refresh rate to override the default on startup, it has to be included on the kernel command line using the "video" parameter.

 

Answer.  To specify the display framebuffer characteristics on the kernel command line, use the "video" parameter in the following format:

 

video=mxcfb:resolution-bitdepth@refresh

 

For example:

 

video=mxcfb:1024x768-24@60

 

sets the framebuffer to 1024x768 resolution, at 24-bit color depth, and 60Hz refresh rate.

 

 Related Products:

 i.MX Applications Processors > i.MX51 Processors > i.MX512, i.MX513, i.MX514, i.MX515, i.MX516

タグ(1)
0 件の賞賛
返信
0 返答(返信)