Sound Solution implementation for IMx6 using PCM1754-Q1 DAC with ESAI Interface

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Sound Solution implementation for IMx6 using PCM1754-Q1 DAC with ESAI Interface

2,118 次查看
vigneshm93
Contributor I

Hi All

Need to design a sound solution with IMx6 ESAI Interface using PCM1754-Q1 DAC

44.1 KHz sample rate audio input (16bit PCM Data) and single channel (right channel) output

Data Format configured in PCM1754-Q1 is 16bit I2S Format

Anybody has tried the solution for the above mentioned specs earlier ?

If not, what will be the ESAI Clock settings (SCK, BCK and LRCK)  for the above mentioned specs ?

ESAI Clock source should be PLL4 and 22.5792MHz System clock frequency is needed as per PCM1754-Q1 Datasheet

标签 (3)
0 项奖励
回复
1 回复

1,998 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Vignesh

esai is supported on i.MX6Q Sabre AI board:

Schematics (5)
Design files for i.MX 6Quad and i.MX 6DualLite CPU1 Cards
Design files for Base Board

http://www.nxp.com/products/software-and-tools/hardware-development-tools/sabre-development-system/s...

Linux driver description is provided in Chapter 28 Advanced Linux Sound Architecture (ALSA) System on a Chip (ASoC)

Sound Driver attached Linux Manual.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复