Some problem about to build android for imx6, according "Android_User's_Guide".

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Some problem about to build android for imx6, according "Android_User's_Guide".

1,524 Views
guanliangding
Contributor III

Hi, all:

     I according "Android_User's_Guide" to build android image. When i lunch the product, the build tools display follow information. And i haven't to patch "android_L5.0.0_1.0.0-ga_omxplayer_source.tar.gz" and "android_L5.0.0_1.0.0-ga_wfdsink_source.tar.gz". I think those is not necessary.

john@ca230:~/myandroid$ lunch sabresd_6dq-user

build/core/product_config.mk:222: *** Can not locate config makefile for product "sabresd_6dq".  Stop.

** Don't have a product spec for: 'sabresd_6dq'

** Do you have the right repo manifest?

    

Labels (1)
Tags (2)
0 Kudos
Reply
2 Replies

1,227 Views
san_0201
Contributor I

hi,

  while i try to apply patch file using below command,

  $c_patch /opt/android_M6.0.1_2.1.0_source/code/M6.0.1_2.1.0/ imx_M6.0.1_2.1.0

   I am getting error:

   Creating NEW gits - external/linux-firmware-imx
   Error! Fail to git commit dummy /home/myandroid/external/linux-firmware-imx

   Please,help me for create the successful patch

 

 

Thanks,

0 Kudos
Reply

1,256 Views
Yuri
NXP Employee
NXP Employee

Hello,

  According to section 6 (Freescale Extended Feature Packages) of
“Android_Release_Notes.pdf”:


“Available for the release are several packages to extend the base Android
Multimedia features. For more information and details about any of the below
packages, please send inquiry to "L2manager-android@freescale.com".


This concerns Extended multimedia feature package and Wi-Fi Display Sink
feature package.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply