Some USB storage devices only work through external hub

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Some USB storage devices only work through external hub

1,308件の閲覧回数
chrgrff1
Contributor II

Hello,

I have an i.MX6Q on a custom baseboard. USB is connected via the USB Host interface.

When directly connected, I have a subset of USB drives which do not "work well." I get "EHCI Timed Out on Token" errors when reading from U-Boot, and in Linux the drives will sporadically disconnect-reconnect.

If I connect an external un-powered USB hub (testing with an Anker 4-port hub) to the i.MX6Q USB Host port, all of the drives work great through the hub.

I've seen similar discussions in the community with solutions about changing load address in U-Boot, etc. but they don't seem to apply here.

Anyone experience anything similar? Thank you.

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,250件の閲覧回数
b36401
NXP Employee
NXP Employee

Please try to connect device with shorter USB cable. Long cable may cause some issues on high speed.

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信