Some Porblems about RPMsg initialize

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Some Porblems about RPMsg initialize

2,551件の閲覧回数
jingyangxie
Contributor V

static void PingPongTask (void* param)
{
    int result;
    struct remote_device *rdev = NULL;
    struct rpmsg_channel *app_chnl = NULL;
    THE_MESSAGE msg = {0};
    int len;

    /* Print the initial banner */
    PRINTF("\r\nRPMSG PingPong FreeRTOS RTOS API Demo...\r\n");

    PRINTF("RPMSG Init as Remote\r\n");
    result = rpmsg_rtos_init(0 /*REMOTE_CPU_ID*/, &rdev, RPMSG_MASTER, &app_chnl);
    assert(0 == result);

    PRINTF("Name service handshake is done, M4 has setup a rpmsg channel [%d ---> %d]\r\n", app_chnl->src, app_chnl->dst);

    while (true)
    {
        /* receive/send data to channel default ept */
        result = rpmsg_rtos_recv(app_chnl->rp_ept, &msg, &len, sizeof(THE_MESSAGE), NULL, 0xFFFFFFFF);
        assert(0 == result);
        PRINTF("Get Data From Master Side : %d\r\n", msg.DATA);
        msg.DATA++;
        result = rpmsg_rtos_send(app_chnl->rp_ept, &msg, sizeof(THE_MESSAGE), app_chnl->dst);
        assert(0 == result);
    }

    /* If destruction required */
    /*
    PRINTF("\r\nMessage pingpong finished\r\n");

    rpmsg_rtos_deinit(rdev);
    */
}

as above ,When I run the pingpong example,the app_chnl->src is 0,and the app_chnl->dst is 1024,why is it ,I don't understand.

ラベル(2)
0 件の賞賛
返信
1 返信

2,228件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

!Hi jingyang

RPMsg Master (Cortex-A9 Linux OS) and Remote (Cortex-M4 FreeRTOS

OS) perform a name service handshake to create the communication channel. The M4 channel address is

1, and the A9 channel address is 1024. Please refer to attached document for Demo details.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信