Hi, every body.
------------------------------------------
i.mx6solo sabresd board
Kernel. 3.14.52
ubuntu 14.04
-----------------------------------------
When I download linux image file with use MFG-TOOLS, I have some error.
mfg-tools version also 3.14.52 .
--------------------------------------------------------------------------------------------------------------------------
U-Boot 2015.04-imx_v2015.04_3.14.52_1.1.0_ga+g6cf684a (Dec 05 2015 - 02:02:52)
CPU: Freescale i.MX6SOLO rev1.2 at 792 MHz
CPU: Temperature 46 C
Reset cause: POR
Board: MX6-SabreSD
I2C: ready
DRAM: 1 GiB
PMIC: PFUZE100 ID=0x10
MMC: FSL_SDHC: 0, FSL_SDHC: 1, FSL_SDHC: 2
*** Warning - bad CRC, using default environment
No panel detected: default to Hannstar-XGA
Display: Hannstar-XGA (1024x768)
In: serial
Out: serial
Err: serial
switch to partitions #0, OK
mmc2(part 0) is current device
Net: FEC [PRIME]
Error: FEC address not set.
Boot from USB for mfgtools
Use default environment for mfgtools
Run bootcmd_mfg: run mfgtool_args;bootz ${loadaddr} ${initrd_addr} ${fdt_addr};
Hit any key to stop autoboot: 0
Kernel image @ 0x12000000 [ 0x000000 - 0x521260 ]
## Loading init Ramdisk from Legacy Image at 12c00000 ...
Image Name: fsl-image-mfgtool-initramfs-imx6
Image Type: ARM Linux RAMDisk Image (gzip compressed)
Data Size: 7508220 Bytes = 7.2 MiB
Load Address: 00000000
Entry Point: 00000000
Verifying Checksum ... OK
## Flattened Device Tree blob at 18000000
Booting using the fdt blob at 0x18000000
Using Device Tree in place at 18000000, end 1800d9b2
switch to ldo_bypass mode!
Starting kernel ...
--------------------------------------------------------------------------------------------------------------------------------------------
Do not proceed download.
What problem am i have?
How to solve this problem?
Original Attachment has been moved to: MfgTool.log.zip
Original Attachment has been moved to: mfgtools-err.log.zip
Hi Hanseung
sabresd board has i.MX6DL processor, for custom board with i.MX6S processor
it is necessary to run ddr test
https://community.freescale.com/docs/DOC-105652
find new calibration coefficients and rebuild mfg tools, please refer
to attached Yocto Guide sect.6.2 Manufacturing Tool, MFGTool
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------