Software code to enable software watch dog timer of imx6ul proceaaor

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Software code to enable software watch dog timer of imx6ul proceaaor

1,977件の閲覧回数
dhanushdhanu
Contributor I

I want the software code to enable the software watchdog timer of imx6ul

ラベル(1)
タグ(1)
0 件の賞賛
返信
2 返答(返信)

1,875件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  Customers can use i.MX 6UL SDK examples. Look at

\SDK_2.2_MCIM6UL\boards\evkmcimx6ul\driver_examples\wdog\wdog.c  

https://www.nxp.com/webapp/Download?colCode=SDK2.2_iMX6UL_WIN&appType=license&location=null 

i.MX Software | NXP 

 

Have a great day,

Yuri.

 

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

0 件の賞賛
返信

1,874件の閲覧回数
kunalkotecha1
Senior Contributor II

Hi dhanushdhanu@embdestech.com,

You can refer to the Section 2.11 for Enabling the Watchdog feature and Section 9.1.5 for unit testing the watchdog use case from "i.MX Reference Manual".

Please find the attachment for the same.

Regards,

Kunal

0 件の賞賛
返信