Software Upgrade through USB

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Software Upgrade through USB

6,594 次查看
kishorepoojari
Contributor III

Hello All,

           We are working on I.Mx233 processors and freescale provided B.S.P . As per the new requirement we have to upgrade the software through USB (previously we used SD card ).

Hence we have to implement all USB OTG diver in Bootloader ,

whether i.mx233 and freescale provided B.S.P will support for the same....?

Regards,

Kishore P

标签 (1)
0 项奖励
回复
8 回复数

6,073 次查看
igorpadykov
NXP Employee
NXP Employee

Hi kishore

in eboot one can download images to NAND with PB help, please

refer to attached WinCE Guide sect.5.5 Configuring USB Serial Connection

for Downloading and Debugging, sect.5.3.2 Burn EBOOT onto NAND flash using PB.

Otherwise one can use MFG Tools.

Best regards

igor

0 项奖励
回复

6,073 次查看
kishorepoojari
Contributor III

Hello igor,

   Problem with the our requirement is device will be fixed , we can't remove it for upgrade (If any update required) . Hence we are planning to implement USB OTG in the bootloader(whether it is possible in imx233 and win ce 6.0 ).

Regards,

Kishore P

0 项奖励
回复

6,073 次查看
igorpadykov
NXP Employee
NXP Employee

Hi kishore

USB OTG is supported in eboot bootloader

and usage is described in this document.

~igor

0 项奖励
回复

6,073 次查看
kishorepoojari
Contributor III

Hello igor,

  Please attach the document (USB OTG in eboot).

Regards,

Kishore P

0 项奖励
回复

6,073 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Kishore

it is attached in answer from

in general one can use eboot sources and write own custom application

for nand image update through usb.

0 项奖励
回复

6,073 次查看
YanjunLuo
Contributor IV

Hi Kishore,

Why not boot a Linux for upgrade? I did it for many years, it's much easier than bootloader.

Regards,

Yanjun Luo.

0 项奖励
回复

6,073 次查看
kishorepoojari
Contributor III

Hello Yanjun Luo,

  Current we are working on windows C.E 6.0 O.S ,  Is it possible that in Bootloader only device shall be USB OTG mode and copy the firmware from USB to NAND flash.

Regards,

Kishore P

0 项奖励
回复

6,073 次查看
YanjunLuo
Contributor IV

Hi Kishore,

Sorry I know nothing about WINCE.

Regards,

Yanjun Luo.

0 项奖励
回复