Smart DMA Usage

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Smart DMA Usage

2,567件の閲覧回数
adityanagal
Contributor III

Hi ,

Please suggest for below questions :

Q1 As per the Reference manual ,  it seems like Smart DMA  can be used while using UART. Is it right ?

Q2  Can we also turn off the Smart DMA while dealing with External memory interfaces like ecSPI with EEPROM ?

Regards,

Aditya Nagal

0 件の賞賛
返信
1 返信

2,237件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Aditya

1. right

2. yes

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信