Smart DMA Usage

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Smart DMA Usage

2,575 次查看
adityanagal
Contributor III

Hi ,

Please suggest for below questions :

Q1 As per the Reference manual ,  it seems like Smart DMA  can be used while using UART. Is it right ?

Q2  Can we also turn off the Smart DMA while dealing with External memory interfaces like ecSPI with EEPROM ?

Regards,

Aditya Nagal

0 项奖励
回复
1 回复

2,245 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Aditya

1. right

2. yes

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复