Slow VGA display performance on iMX53 QSB EC7 platform

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Slow VGA display performance on iMX53 QSB EC7 platform

923 次查看
bdp42
Contributor IV

Hi,

I am running Windows Embedded Compact 7 on an iMX53 Quick Start Board platform. The BSP is based on the SABRE ARD board ported to the QSB.

I am using an external VGA display (DI1 set as primary panel) and the display performance is slow. For example, entering 'dir' at the command prompt takes about 3 seconds to output a list of 25 files. I've checked the various clocks ( CPU, DRAM, etc ) and they are set at the max values and I believe I've selected all of the appropriate catalog items.

This seems very slow and I assume this is not normal behaviour. Can anyone suggest possible causes of this problem or specific areas that could be investigated?

Thanks

Bruno

标签 (1)
标记 (2)
0 项奖励
回复
1 回复

795 次查看
Philip_FSL
Contributor IV

You might check that there aren't spurious interrupts.  Also, refer to the documentation and turn off GDI acceleration to see if that has an impact.

0 项奖励
回复