Hi,
I have not tried the non USB camera.
We are also able to do video call without an issue for VGA camera.
I have connected HD camera (USB) , which creates an issue after 10 to 15 min of video call.
Temperature detail is as below.
After boot completed :- 50 C
Skype Video call, Call is not received at other end, Just preview your camera in screen. :- 60 C
Skype video call, with both video display :- 67 C
Skype video call, with both video display after 1 min :- 75 C
Skype video call, with both video display after 5 min :- 80 C
If you look at the CPU utilization during this process
Skype takes around 50 % of CPU.
Media server takes around 35 to 40 % of CPU.
Thanks
Saurabh