Simultaneous firmware upgrade using MfgTools with imx233

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Simultaneous firmware upgrade using MfgTools with imx233

1,003件の閲覧回数
paolomartinetti
Contributor I

Hi everybody,

i have a question about mfgtools:

is there any way to load one or more devices (imx233) simoultaneously with different profiles using mfgtools?

This question arises from the need to load different encrypted firmwares on different devices in a production environment.

Thanks in advance

Paolo

ラベル(1)
0 件の賞賛
返信
1 返信

901件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi Paolo,

Please check the Mfgtool operation manual documentation, in case of the latest mfgtool version 4.1v  refers that no more than 4 devices are allowed to be connected simultaneously. you need to check this manual according to the version  you are using, since previous mfgtools version are able to update firmware, in less than 4 devices

Have a great day,

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信