Simultaneous Audio Capture & Playback in IMX6

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Simultaneous Audio Capture & Playback in IMX6

2,455件の閲覧回数
himanshugusain
Contributor III

We have 2 different sound cards configured  Audio Codec & BT SCO

We are working on the usecase where we record from Bluetooth interface & simultaneously sends that data out

through Audio Codec (external speaker).

How can we verify this functionality from the avaliable command line utility like tinycap & tinyplay .

Or Is there any command line utility which can be used to test this functionality

0 件の賞賛
返信
1 返信

2,109件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi himanshu

for basic codec testing one can try unit tests (folder /mxc_sound_test)

and dscription in attached Linux Manual sect.28.5 Unit Test

imx-test
www.nxp.com/lgfiles/NMG/MAD/YOCTO/imx-test-5.7.tar.gz

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信