Simple Audio setup in Linux iMX6

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Simple Audio setup in Linux iMX6

4,575件の閲覧回数
erezsteinberg
Contributor IV

Hello experts,

I have a simple audio setup on my board. I have an external DAC+Amplifier that connects to iMX6 over I2S and to a speaker (Mono).

There are no controls for the 'codec' -- it just plays what is sent over I2S.

There's no headphone or microphone... just one output with no configuration options.

(iMX6 is I2S Master, for clocking)

Can I use 'simple-audio-card' or something else to easily set up such a configuration?

Regards,

Erez

ラベル(2)
タグ(3)
0 件の賞賛
返信
1 返信

3,270件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Erez

I am afraid not, just for quick reference please look at attached

documents Chapters Porting Audio Codecs to a Custom Board.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信