Similar i.MX6Q NAND boot issues

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Similar i.MX6Q NAND boot issues

863 Views
anthonyczarneck
Contributor I

I've been trying to get the i.MX6Q to boot from NAND on a custom board, but I've been having some trouble.

In this discussion, it looked like the a lot of information about the boot procedure was able to be read from the first 256 bytes of the boot log buffer.

Is there anyone that can interpret this or point me to where it might be documented?

S:0x000000D0:  0x00902190

S:0x00902190:    0x01    0x00    0x01    0x00    0xF0    0x00    0x02    0x00    0x00    0x00    0x03    0x00    0x01    0x00    0x04    0x00    0x00    0x00    0x0C    0x00    0x00    0x00   

S:0x009021A6:    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00   

S:0x009021BC:    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00   

S:0x009021D2:    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00   

S:0x009021E8:    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00   

S:0x009021FE:    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00   

S:0x00902214:    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00   

S:0x0090222A:    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00   

S:0x00902240:    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00   

S:0x00902256:    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00   

S:0x0090226C:    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00   

S:0x00902282:    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00   

0 Kudos
Reply
1 Reply

725 Views
Yuri
NXP Employee
NXP Employee

Boot ROM Code has a data logger : “pu_irom_log_buffer” at 0x00902190, 256 bytes.

I will send You codes directly.


Also one can use two Linux log files to view boot problem :

/var/log/bootstrap.log 

/var/log/dmesg


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply