Silicon version for i.MX25

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Silicon version for i.MX25

ソリューションへジャンプ
2,366件の閲覧回数
fmvalero
Contributor II

Hi all,

I designed a custom board based on i.MX25 PDK, which is working fine. The silicon version of this processor is 1.1. For my new design (similar to the previous), I am going to use a i.MX253 processor with silicon version 1.2. I have found no information on what this could mean for my new design. Is there any hardware or software issue I should consider over the previous silicon version?

Otherwise, the last version of ATK tool has only two options for i.MX25 processors: i.MX25_TO1.0 or i.MX25_TO1.1. Can I still use ATK for flashing Nand Flash with the silicon version 1.2?

Thanks,

Fernando.

ラベル(1)
0 件の賞賛
返信
1 解決策
2,267件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Fernando

silicon version 1.2 fixed SRTC erratum, in other aspects

it is the same as 1.1. ATK tool works well with it.

IMX25CE Chip Errata for the i.MX25

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,268件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Fernando

silicon version 1.2 fixed SRTC erratum, in other aspects

it is the same as 1.1. ATK tool works well with it.

IMX25CE Chip Errata for the i.MX25

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
2,267件の閲覧回数
fmvalero
Contributor II

OK. Thank you, chip

0 件の賞賛
返信