Silex SDCAN module tests

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Silex SDCAN module tests

3,442件の閲覧回数
seshpadm
Contributor I

Hi,

I'd appreciate if anyone can share basic functionality/performance, WiFi driver performance/memory and other test results for Silex SDCAN module with i.MX6 or any other freescale platform.

Thanks,

SeshPad

ラベル(2)
0 件の賞賛
返信
3 返答(返信)

3,194件の閲覧回数
seshpadm
Contributor I

Hi Yuji,

Thank you for providing performance related data w.r.t. data transfer rates. I am trying to assess multiple radio module vendors and we are looking at multiple criteria like power consumption, data rates, handover times, memory footprint, driver execution times etc.. on i.MX6 processor. Any data relevant to these or anything that differentiates Silex from other radio modules will be of great help.

Regards,

SeshPad

0 件の賞賛
返信

3,194件の閲覧回数
YS
Contributor IV

Sesh,

Please contact silex america technical support.

I cannot disclose too much detail here. You may need to sign NDA for more detailed data.

Best Regards,

0 件の賞賛
返信

3,194件の閲覧回数
YS
Contributor IV

This is not an official performance data, neither max possible performance

measured in ideal condition. This is just an example what I saw on my desktop with

iperf (TCP) throughput, in moderately congested radio environment / close

distance (4ft) from consumer-class 802.11n Access Point.

5GHz HT40 transmit 48Mbps

5GHz HT40 receive 52Mbps

2.4GHz HT20 transmit 20Mbps

2.4GHz HT20 receive 25Mbps

Note that you must configure clock governor to "performance" on iMX6 Ubuntu Linux.

echo performance > /sys/devices/system/cpu/cpu0/cpufreq/scaling_governor

echo performance > /sys/devices/system/cpu/cpu1/cpufreq/scaling_governor

echo performance > /sys/devices/system/cpu/cpu2/cpufreq/scaling_governor

echo performance > /sys/devices/system/cpu/cpu3/cpufreq/scaling_governor


The power-on default is "automatic", which significantly reduce CPU performance.

For functionality, do you have specific feature looking for?