Signing image with second SRK1 does not work for me, while first SRK0 works fine.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Signing image with second SRK1 does not work for me, while first SRK0 works fine.

ソリューションへジャンプ
4,028件の閲覧回数
abid_khan1
Contributor II

I have same problem, signing image with second SRK1 does not work for me, while first SRK0 works fine.

Here are my CSF file to make sign image.

####For SRK0 ( which works)####

[Header]
Version = 4.0
Hash Algorithm = sha256
Engine Configuration = 0
Certificate Format = X509
Signature Format = CMS

[Install SRK]
File = "../crts/SRK_1_2_3_4_table.bin"
Source index = 0 # Index of the key location in the SRK table to be installed

[Install CSFK]
# Key used to authenticate the CSF data
File = "../crts/CSF1_1_sha256_4096_65537_v3_usr_crt.pem"

[Authenticate CSF]


[Install Key]
# Key slot index used to authenticate the key to be installed
Verification index = 0
# Target key slot in HAB key store where key will be installed
Target index = 2
# Key to install
File = "../crts/IMG1_1_sha256_4096_65537_v3_usr_crt.pem"

[Unlock]
Engine = CAAM
Features = RNG

[Authenticate Data]
# Key slot index used to authenticate the image data
Verification index = 2
# Sign padded SPL starting at the IVT through to the end with
# length = $FILESIZE (padded SPL length)
# This covers the essential parts: IVT, boot data and DCD.
# Blocks have the following definition:
# Image block start address on i.MX, Offset from start of image file,
# Length of block in bytes, image data file

# Address Offset Length Data File Path
Blocks = 0x00907400 0x000 0x6c00 "SPL-pad.bin"

#####CSF file for SRK1, it does not work,######

[Header]
Version = 4.0
Hash Algorithm = sha256
Engine Configuration = 0
Certificate Format = X509
Signature Format = CMS

[Install SRK]
File = "../crts/SRK_1_2_3_4_table.bin"
Source index = 1 # Index of the key location in the SRK table to be installed

[Install CSFK]
# Key used to authenticate the CSF data
File = "../crts/CSF2_1_sha256_4096_65537_v3_usr_crt.pem"

[Authenticate CSF]


[Install Key]
# Key slot index used to authenticate the key to be installed
Verification index = 0
# Target key slot in HAB key store where key will be installed
Target index = 2
# Key to install
File = "../crts/IMG2_1_sha256_4096_65537_v3_usr_crt.pem"

[Unlock]
Engine = CAAM
Features = RNG

[Authenticate Data]
# Key slot index used to authenticate the image data
Verification index = 2
# Sign padded SPL starting at the IVT through to the end with
# length = $FILESIZE (padded SPL length)
# This covers the essential parts: IVT, boot data and DCD.
# Blocks have the following definition:
# Image block start address on i.MX, Offset from start of image file,
# Length of block in bytes, image data file

# Address Offset Length Data File Path
Blocks = 0x00907400 0x000 0x6c00 "SPL-pad.bin"

Is any thing missing or incorrect in CSF file for SRK1? Thanks.

Here are HAB events report return by "hab_status".

U-Boot > hab_status

Secure boot disabled

Reporting HAB events HAB_STS_ANY

HAB Configuration[0xf0]: HAB_CFG_OPEN
HAB State[0x66]: HAB_STATE_NONSECURE
0: hStatus 0xf0 bytes 20

--------- HAB Event 1 -----------------
event data:
Status[0x33]: HAB_FAILURE
Reason[0x0f]: HAB_INV_INDEX
Context[0xc0]: HAB_CTX_COMMAND
Engine[0x00]: HAB_ENG_ANY
Cmd[0xbe]: HAB_CMD_INS_KEY
KeyIdx[0x03]
Protocol[0x17]: Unknown
Engine[0x01]: Unknown, Cfg[0x00]: Unknown
authentication data address relative to CSF start
0xbe 0x00 0x0c 0x00 0x03 0x17 0x01 0x00
0x00 0x00 0x00 0x50
1: hStatus 0xf0 bytes 20

--------- HAB Event 2 -----------------
event data:
Status[0x33]: HAB_FAILURE
Reason[0x0f]: HAB_INV_INDEX
Context[0xc0]: HAB_CTX_COMMAND
Engine[0x00]: HAB_ENG_ANY
Cmd[0xbe]: HAB_CMD_INS_KEY
KeyIdx[0x03]
Protocol[0x17]: Unknown
Engine[0x01]: Unknown, Cfg[0x00]: Unknown
authentication data address relative to CSF start
0xbe 0x00 0x0c 0x00 0x03 0x17 0x01 0x00
0x00 0x00 0x00 0x50
2: hStatus 0xf0 bytes 20

--------- HAB Event 3 -----------------
event data:
Status[0x33]: HAB_FAILURE
Reason[0x0c]: HAB_INV_ASSERTION
Context[0xa0]: HAB_CTX_ASSERT
Engine[0x00]: HAB_ENG_ANY
Event 1 Address: 0x00907400
Length: 0x00000020

3: hStatus 0xf0 bytes 20

--------- HAB Event 4 -----------------
event data:
Status[0x33]: HAB_FAILURE
Reason[0x0c]: HAB_INV_ASSERTION
Context[0xa0]: HAB_CTX_ASSERT
Engine[0x00]: HAB_ENG_ANY
Event 1 Address: 0x0090742c
Length: 0x00000060

4: hStatus 0xf0 bytes 20

--------- HAB Event 5 -----------------
event data:
Status[0x33]: HAB_FAILURE
Reason[0x0c]: HAB_INV_ASSERTION
Context[0xa0]: HAB_CTX_ASSERT
Engine[0x00]: HAB_ENG_ANY
Event 1 Address: 0x00907420
Length: 0x00000001

5: hStatus 0xf0 bytes 20

--------- HAB Event 6 -----------------
event data:
Status[0x33]: HAB_FAILURE
Reason[0x0c]: HAB_INV_ASSERTION
Context[0xa0]: HAB_CTX_ASSERT
Engine[0x00]: HAB_ENG_ANY
Event 1 Address: 0x00908000
Length: 0x00000004

6: hStatus 0xf0 bytes 20

--------- HAB Event 7 -----------------
event data:
Status[0x33]: HAB_FAILURE
Reason[0x0c]: HAB_INV_ASSERTION
Context[0xa0]: HAB_CTX_ASSERT
Engine[0x00]: HAB_ENG_ANY
Event 1 Address: 0x80841000
Length: 0x00000020

7: hStatus 0xf0 bytes 20

--------- HAB Event 8 -----------------
event data:
Status[0x33]: HAB_FAILURE
Reason[0x0c]: HAB_INV_ASSERTION
Context[0xa0]: HAB_CTX_ASSERT
Engine[0x00]: HAB_ENG_ANY
Event 1 Address: 0x80800000
Length: 0x00000004

1 解決策
3,851件の閲覧回数
abid_khan1
Contributor II

Thank you Yuri. The other keys SRK1-3 also work for me now.

The problem was that only  first SRK0 was present in my SRK_1_2_3_4_table.bin file, reason was spaces in between SRK certificates keys files after "," in srktool cmd line to generate SRK_1_2_3_4_table.bin.

One must pay attention to the instruction in srktool --help that mention

"Certificate filenames must be separated by a ','with no spaces"

元の投稿で解決策を見る

5 返答(返信)
3,851件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

    What is part number of the i.MX device, used in the case? 

Regards,

Yuri.

0 件の賞賛
返信
3,851件の閲覧回数
abid_khan1
Contributor II

Thank you for quick response.

I used IMX6Q based Solidrun HummingBoard2 and following is /proc/cpuinfo

processor : 0
model name : ARMv7 Processor rev 10 (v7l)
BogoMIPS : 3.00
Features : half thumb fastmult vfp edsp neon vfpv3 tls vfpd32
CPU implementer : 0x41
CPU architecture: 7
CPU variant : 0x2
CPU part : 0xc09
CPU revision : 10

processor : 1
model name : ARMv7 Processor rev 10 (v7l)
BogoMIPS : 3.00
Features : half thumb fastmult vfp edsp neon vfpv3 tls vfpd32
CPU implementer : 0x41
CPU architecture: 7
CPU variant : 0x2
CPU part : 0xc09
CPU revision : 10

processor : 2
model name : ARMv7 Processor rev 10 (v7l)
BogoMIPS : 3.00
Features : half thumb fastmult vfp edsp neon vfpv3 tls vfpd32
CPU implementer : 0x41
CPU architecture: 7
CPU variant : 0x2
CPU part : 0xc09
CPU revision : 10

processor : 3
model name : ARMv7 Processor rev 10 (v7l)
BogoMIPS : 3.00
Features : half thumb fastmult vfp edsp neon vfpv3 tls vfpd32
CPU implementer : 0x41
CPU architecture: 7
CPU variant : 0x2
CPU part : 0xc09
CPU revision : 10

Hardware : Freescale i.MX6 Quad/DualLite (Device Tree)
Revision : 63015
Serial : 0000000000000000

3,851件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  The issue was checked with 6Q Sabresd board with CST3.1 and L4.14.78_1.0.0_GA uboot. SRK2 works.

Please try using NXP SDP/B board with NXP U-boot.

Regards,

Yuri.

0 件の賞賛
返信
3,852件の閲覧回数
abid_khan1
Contributor II

Thank you Yuri. The other keys SRK1-3 also work for me now.

The problem was that only  first SRK0 was present in my SRK_1_2_3_4_table.bin file, reason was spaces in between SRK certificates keys files after "," in srktool cmd line to generate SRK_1_2_3_4_table.bin.

One must pay attention to the instruction in srktool --help that mention

"Certificate filenames must be separated by a ','with no spaces"

3,851件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  please double check  SRK_1_2_3_4_table.bin's size;  are all 4 SRK keys in the SRK table?

  What is key length (maybe 2048 bit)? 

Regards,

Yuri.