Shutting down the Cortex M4 core on the iMX7d processor

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Shutting down the Cortex M4 core on the iMX7d processor

2,496 次查看
cnapolitano
Contributor I

Our device is currently not utilizing the Cortex M4 core on the i.MX7d processor. Is there any means (GPIO, SMBus,etc.) to power off the Cortex M4 core?

标签 (1)
标记 (2)
2 回复数

2,396 次查看
karangajjar
Senior Contributor II

Hi Cameron Napolitano,

As mentioned in the i.MX7D RM section 4.2.5 Cortex-M4 Boot requirement, Cortex-A7 is responsible for enabling and providing clock to Cortex-M4, please see the image below:

Screenshot from 2020-01-22 12-23-35.png

Taking clue from the last point, using the SRC_M4RCR(M4 Reset Control Register) register's 3rd bit (ENABLE_M4) we can enable/disable M4.

Regards,

Karan Gajjar

2,396 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

good!