Shudown and PowerOff Commands are not working as expected

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Shudown and PowerOff Commands are not working as expected

1,281 次查看
akashnair316
Contributor I

Hi,

Currently we are facing a issue with shutdown and poweroff commands. When any one of this command is entered from our command line, the system it gets re-started by itself rather than going into power-off mode or shut down mode. The same we evaluated with im6ull-EVK it works as expected in it but it is not working in our custom board. 
Also, when halt command is entered in our custom board it also works as expected but shutdown and poweroff are not working as expected. We are using pf3001 in our custom board. 
So,
(i) Do I need to configure/takecare any PIN for getting these 2 commands properly?  
(ii) Also what will be reason for this behaviour?
标记 (3)
0 项奖励
回复
1 回复

1,222 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Akash

one can recheck pmic pwron connection, look at imx6ull-9x9-evk.dts

imx6ull-9x9-evk.dts\dts\boot\arm\arch - linux-imx - i.MX Linux kernel 

Also some third party boards use pf3000 with i.mx6ul

ConnectCore® for NXP i.MX6 UltraLite - Linux SOM | Digi International 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复