Sharing boot_cfg lines

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Sharing boot_cfg lines

跳至解决方案
2,727 次查看
jautry
Contributor IV

I noted on the eval board that Boot-Cfg input lines to the processor MIMXRT 1062  were shared.  Is it possible to share these lines since they are only accessed at startup for config data?  Is the way to do this is to start with them configured for Boot-Cfg and after boot changing the line configuration?

0 项奖励
回复
1 解答
2,709 次查看
Yuri
NXP Employee
NXP Employee

@jautry 
Hello,

  The default pins state are configured after boot configuration is latched.

Regards,
Yuri

 

在原帖中查看解决方案

0 项奖励
回复
3 回复数
2,721 次查看
Yuri
NXP Employee
NXP Employee

@jautry 
Hello,

  Section 9.4.2 (GPIO boot overrides) of the RM contains information about the boot override pins.

https://www.nxp.com/webapp/Download?colCode=IMXRT1060RM

  After boot these pins can be used for other functionality.
Use i.MX Pins tool for possible configurations.

https://www.nxp.com/pages/pins-tool-for-i.mx-application-processors:PINS-TOOL-IMX

Regards,
Yuri.

0 项奖励
回复
2,715 次查看
jautry
Contributor IV

I just want to make sure.  The config tool lists the GPIO as the default at power up but not the config option.  So the default is actually the config option for reading the boot configs and then the mux is executed to direct the pins to proper configuration.  We do not have to specifically define the pin for config option.

0 项奖励
回复
2,710 次查看
Yuri
NXP Employee
NXP Employee

@jautry 
Hello,

  The default pins state are configured after boot configuration is latched.

Regards,
Yuri

 

0 项奖励
回复