Several issues after loading supercap higher than 2.3V on i.MX7D board

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Several issues after loading supercap higher than 2.3V on i.MX7D board

1,637 次查看
dm2
Contributor I

Several issues after loading supercap higher than 2.3V on i.MX7D board.

Brief description:

  • With the latest build 114 we enabled the charging of the supercap, i. e.:

    --> PF3000: in register 0xA1 (COINCTL) VCOIN was set to 111 (Voltage = 3,3V and COINCHEN = 1).
    --> Supercap is now charged correctly up to the selected load voltage 3,3V.

    Issue:

    As soon as the voltage of the supercap is higher than 2,3V and the power supply voltage is turned off the unit does not boot anymore. Also, we don't get any output on the serial debug interface anymore, the RESET-key has no function and further on flashing the firmware does not work, too.

    Actual results of our research:

    --> VIN_5V OK --> PMIC_PWR (3,7V) OK --> VLDO_3V3, MX7_RST_B and POR_B NOT OK approx. 1,58V (should be 3,3V)

    --> RESET input POR_B of the i.MX7D is on voltage level 1,58V --> Processor is in Reset?

    --> When the supercap will be discharged to less than 2,30V, the EWIO2 unit boots normally as known before and all voltages VLDO_3V3, MX7_RST_B and POR_B are set to 3,3V again. The RESET key, the serial debug interface and firmware flashing also works again.
标签 (1)
0 项奖励
回复
2 回复数

1,549 次查看
gusarambula
NXP TechSupport
NXP TechSupport

Hello Dieter Möhrle,

I was reviewing this case and further information on your hardware such as schematics for your board may be needed. Would you please open a support Case including your schematic and referencing this thread so that follow up may be provided? This way you don’t need to share your schematic publicly.

Regards,

0 项奖励
回复

1,549 次查看
dm2
Contributor I

Hello,

I already opened a case and the schematics have been attached to it. A

guy called Jozef is already in charge of it...

Thank you,

Dieter

Am 05.03.2020 um 18:13 schrieb gusarambula:

>

NXP Community

<https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>

>

Re: Several issues after loading supercap higher than 2.3V on

i.MX7D board

reply from gusarambula

<https://community.nxp.com/people/gusarambula?et=watches.email.thread>

in /i.MX Processors/ - View the full discussion

<https://community.nxp.com/message/1279238?commentID=1279238&et=watches.email.thread#comment-1279238>

>

0 项奖励
回复