Setup and Build the Community Yocto Project Dora BSP for Freescale i.MX6

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Setup and Build the Community Yocto Project Dora BSP for Freescale i.MX6

5,283 次查看
javierw
Contributor II

I’m try to doing the “bitbake fsl-image-test” for the Setup and Build the Community Yocto Project Dora BSP for Freescale i.MX6.  

Encountered the error in the below image file. 

Appreciate if you could advice how I can proceed from this error.  

Thanks!

 

 

 

标签 (2)
0 项奖励
回复
1 回复

5,205 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Javier

as shows image1.png Ubuntu 16.04 was not validated with that version

of build system, recommended to try on tested Ubuntu 12.04 version and download

packages described in sect.3.1 Host packages attached Yocto Guide.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复