Settings of MMDC MDSCR with programming aid

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Settings of MMDC MDSCR with programming aid

1,513 Views
ko-hey
Senior Contributor II

Hi all

I have a question about following programming aid.

https://community.freescale.com/docs/DOC-105967

In line 183 and 184 of the programming aid, it can set a outout drive strength.

However, there are no discription about it in the reference manual.

Where can user find the description in the reference manual ?

ko-hey

Labels (1)
0 Kudos
Reply
2 Replies

1,312 Views
Yuri
NXP Employee
NXP Employee

Hello,

  The mentioned settings relate to configuring drive strength of

an external DRAM part, therefore please use DRAM datasheet

for more details about Mode Registers.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,312 Views
ko-hey
Senior Contributor II

Hi Yuri

Thank you for your quick response.

I got it.

Ko-hey

0 Kudos
Reply