Settings APP cannot launch in L5.15 desktop

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Settings APP cannot launch in L5.15 desktop

Jump to solution
3,416 Views
kenyroj
Contributor II

Hi All

I tried to build the imx-image-desktop via the manifest: imx-5.15.32-2.0.0_desktop.xml.
Now I tried to launch the Setting APP so I click the Setting icon. After clicking its icon, the mouse pointer shows as busy (spinning) for a few seconds, then the pointer returns to normal, but the app still does not launch. 

I tried another way that enter the 'gnome-control-center' to launch the Setting app and I got following message on console.

gnome-control-center: symbol lookup error: /lib/x86_64-linux-gnu/libwebkit2gtk-4.0.so.37: undefined symbol: gbm_bo_create_with_modifiers2

 Please help to check this issue. Thanks

0 Kudos
Reply
1 Solution
3,271 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi @kenyroj 

This issue is caused by Ubuntu upstream update which you can refer this thread:

https://bugs.launchpad.net/ubuntu/+source/gnome-control-center/+bug/2063476

 

The Linux POC is out of update and the NXP SW team don't plan to continue maintain POC. For future debian support, customer should use flexbuild to deploy debain.

https://github.com/NXP/flexbuild

https://www.nxp.com/docs/en/user-guide/UG10155.pdf


Best Regards
Zhiming

View solution in original post

6 Replies
3,392 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi @kenyroj 

Can you also test imx-5.15.71-2.2.0_desktop.xml?

Best Regards
Zhiming

0 Kudos
Reply
3,366 Views
kenyroj
Contributor II
Hi @Zhiming

Thanks for the reply. I did try the imx-5.15.71-2.2.0_desktop.xml with Ubuntu 22.04.1 LTS. This issue is still existed.

Is there any solution for this?

Thanks
0 Kudos
Reply
3,334 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi @kenyroj 

This issue is caused by Ubuntu upstream update. The Linux POC is out of update and there is no plan to continue maintain POC. For future ubuntu/debian support, customer should use flexbuild to deploy ubuntu or debain.

https://github.com/NXP/flexbuild

https://www.nxp.com/docs/en/user-guide/UG10155.pdf


Best Regards
Zhiming

0 Kudos
Reply
3,348 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi @kenyroj 

 

I am compiling same version and test it on my side, 


Best Regards
Zhiming

3,275 Views
kenyroj
Contributor II
Hi @Zhiming

Could you supply any update about this?
Thanks
0 Kudos
Reply
3,272 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi @kenyroj 

This issue is caused by Ubuntu upstream update which you can refer this thread:

https://bugs.launchpad.net/ubuntu/+source/gnome-control-center/+bug/2063476

 

The Linux POC is out of update and the NXP SW team don't plan to continue maintain POC. For future debian support, customer should use flexbuild to deploy debain.

https://github.com/NXP/flexbuild

https://www.nxp.com/docs/en/user-guide/UG10155.pdf


Best Regards
Zhiming